Skip to main content
Son, Dong-Seong
Associate III
May 30, 2024
Question

The problem of Ethernet with FREERTOS cmsis_v1 on STM32H743

Hi 

I am testing the ethernet with cmsis_v1 on stm32h743 (STM32H743I-EVAL2)

I chose cmsis_v2 and when I pinged the board, the ping was successful.

However, after selecting cmsis_v1, the ping does not work.

Is there something that needs to be configured separately when selecting cmsis_v1?

The current IDE version is 1.15.1, and the firmware package version is v1.11.2.

Can you figure out why it doesn't work when I simply switched from CMSIS v2 to CMSIS v1?

    This topic has been closed for replies.

    2 replies

    ST Employee
    May 31, 2024

    Hello @Son, Dong-Seong ,

    The recommendation will be to follow this example.
    Also be aware that with the newer version of cube when using Cmsis V1 be aware of these issues 
    Allow user to override LWIP_PROVIDE_ERRNO · Issue #1 · STMicroelectronics/stm32_mw_lwip (github.com)
    and don't forget to check for the MPU configuration and the descriptor placement to make this work. this can be found in detail in the attached example.

    Regards 

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Pavel A.
    May 31, 2024

    Recommend to throw the CMSIS crutches away and convert the code to the straight native FreeRTOS calls. This won't leave any room for confusion. Just you and FreeRTOS, nothing else in the middle.