Skip to main content
Tajwar.Chandel
Associate III
October 19, 2022
Question

The Board Part No. B-U585I-IOT02A not getting RESET after pressing the RESET button (B2). The STM32CubeIDE is not getting disconnected after pressing the RESET button. Is this the hardware fault in this board ? Please help to resolve the issue.

..

This topic has been closed for replies.

2 replies

RomainR.
ST Employee
October 19, 2022

Hello @Tajwar.Chandel (Community Member)

Could you be more precise in your statements?

The board is not reset after pressing B2 button (RESET IO of STM32U585) what do you observe?

Does your firmware in flash memory doesn't start or not start ?

Are you in debug mode thru STM32CubeIDE ?

You're expected that the board should disconnect after pressing button, why ?

Best regards,

Romain,

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Tajwar.Chandel
Associate III
November 3, 2022

Hi Romain,

The issue is solved with the help of ST Team INDIA.

Thanks for the responding.

Regards,

Tajwar