Skip to main content
Associate
December 14, 2023
Question

Target not found in STM32CubeIDE.

Target not found in STM32CubeIDE.

When I try to write to the STM MCU from STM32cubeIDE, the following error message is displayed and the MCU cannot be recognized.

「Target no device found

Error in initializing ST-LINK device.

Reasn: No device found on target」

 

The following checks have been performed.
・3.3V is input to VDD, VDDA, VBAT, and VREF+.
・Connect 2.2µF capacitors to VCAP1 and VCAP2.
・The BOOT0 pin should be LOW.

 

One is recognized and the other is not. Both use the same components.
The voltage of the recognized one's VCAP is about 1.2V and the voltage of the unrecognized one's VCAP is about 0V.

How can I solve this problem?



This topic has been closed for replies.

4 replies

Michael E
ST Technical Moderator
December 14, 2023

Hello yyuyu,
Can you specify which board/STM32 you are using?

Best Regards

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
yyuyuAuthor
Associate
December 17, 2023

Thanks for the reply Michael E.

The STM32 I am using is the STM32F2 series.
It is not an evaluation board but a home-made board.

 

Tesla DeLorean
Guru
December 18, 2023

Is the one with 0V on VCAP drawing an excessive amount of current, or none?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
yyuyuAuthor
Associate
December 18, 2023

Thanks for the reply Tesla DeLorean.

No current is flowing in VCAP.