Skip to main content
Associate II
Jul 21, 2025 10:31 AM UTC
Solved

Target not connected and st link not detected

"Hello, I am using a NUCLEO-H7A3ZI-Q board. I flashed two programs successfully, but on the third attempt, it stopped flashing because I accidentally forgot to enable Serial Wire Debug. Now, when I connect a charging cable, it shows 'No target found,' and when I connect a data cable, it shows 'No ST-LINK detected.' Please help.

shared image (1).jpg

Screenshot 2025-07-21 155943.png

This topic has been closed for replies.
MHoll.2
MHoll.2Best answer
Senior III
Jul 21, 2025 10:43 AM UTC

Try setting BOOT0 to High (set Jumper before powering the Board!).

On the NUCLEO-H7A3ZI-Q BOOT0 is on CN11 Pin 7, You can Jump this signal directly to CN11 Pin 5.

MHoll2_0-1753094737571.png

 

3 replies

Andrew Neil
Super User
Jul 21, 2025 10:37 AM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MHoll.2
MHoll.2Best answer
Senior III
Jul 21, 2025 10:43 AM UTC

Try setting BOOT0 to High (set Jumper before powering the Board!).

On the NUCLEO-H7A3ZI-Q BOOT0 is on CN11 Pin 7, You can Jump this signal directly to CN11 Pin 5.

MHoll2_0-1753094737571.png

 

Associate II
Jul 21, 2025 11:29 AM UTC

Hi @Andrew Neil  @MHoll.2 Thanks for reply. Now it is working