Target is not responding, retrying...
The .elf file is built, then I try to download it, and I get all this mess. I believe something is not getting erased from the previous run. I tried openocd, erased the file, but it is still having issues. Any ideas would helpful. ---Randy
STMicroelectronics ST-LINK GDB server. Version 7.14.0
Copyright (c) 2026, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.24.0
-------------------------------------------------------------------
Log output file: C:\Users\Randy\AppData\Local\Temp\STM32CubeProgrammer_a01828.log
ST-LINK SN : 066DFF555278665067093421
ST-LINK FW : V2J49M36
Board : NUCLEO-F411RE
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x431
Revision ID : Rev A
Device name : STM32F411xC/E
NVM size : 512 KBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xD0
Opening and parsing file: ST-LINK_GDB_server_a01828.srec
Memory Programming ...
File : ST-LINK_GDB_server_a01828.srec
Size : 976.000 B
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.319
Verifying...
File size < 32KB legacy verify will be used
Time elapsed during verifying operation: 00:00:00.007
Download verified successfully
Error in executing 'cont' command ...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
GdbSession, Lost target connection, Exiting...
Failed to read registers from target
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Failed to read registers from target
GdbSession, Lost target connection, Exiting...
Shutting down...
Exit.