Switching from STM32H743ZIT (2MB) to STM32H743ZGT (1MB)
We need to start building with the 1MB STM32H743ZGT while all the development has been done for the 2MB STM32H743ZIT. As far as I can tell I cannot change the micro in the .iot file for file generation even though the pin assignments and peripherals seem to exactly the same.
Do I have to create a new .ioc file (and new project), re-setup all the pin assignments and peripheral settings, and import in all the existing source files or is there a simpler way to do this and still use the .ioc file for code generation?