Switching between Nucleo and custom board
I used a Nucleo F439ZI to develop initial software (with a custom daughterboard) and now have redesigned the whole lot onto a single board with the STM32 MCU. I'd like to remain able to support both boards in my Cube project as the nucleo one is much easier to modify.
I used the pinout -> compatible MCU selector in Cube to find an MCU which digikey stocked and which was the cheapest pinout compatible which met my needs which found the F429ZET6. I'd have imagined that thanks to the HAL I would simply need to switch "Build configuration" or similar to go between them but this doesn't seem to work it sems I need to completely retarget, code generate the project. Am I missing something obvious? This seems to be the design journey the software encourages me to take.
Did I make a mistake in not using the identical MCU (STM32F439ZIT6) to the one on the Nucleo Board?