Skip to main content
Associate
November 8, 2024
Solved

Strange logic problem after compilation in CUBE IDE 1.14.1

Hi all,

    basic info:

    stm32 CUBE IDE v1.14.1

    PC: Win10 64bit

    MCU:STM32G0B1CC

 

    In my code, there are two functions to control the battery to enter charge mode from init mode, when the battery receive a command. Check_AuthCmdToCHG()will set CANOpenStruct.flag_authCmdGotoCHG to STD_TRUE and set CANOpenStruct.sendTPDOInfo STD_TRUE. 

   normally,after CANOpenStruct.flag_authCmdGotoCHG be set to  STD_TRUE , CheckFlag_InitGotoCHG() will make state machine FSM goes to charge mode.

   But it's very strange, i send a command to MCU, then I receive TPDO info from CAN bus, this means CANOpenStruct.sendTPDOInfo already be set to STD_TRUE. however  CANOpenStruct.flag_authCmdGotoCHG and CheckFlag_InitGotoCHG() are not work!

   When I examined the code, I couldn't find the cause. Therefore, I wrote a test function Test_CANCmd() ready to read CANOpenStruct.flag_authCmdGotoCHG and CANOpenStruct.sendTPDOInfo out, the other did not modify any code!  I compile the code and burn it like before. Then something amazing happened. Everything worked!

   is there anyone can explain this? The Test_CANCmd()function just uses the value of CANOpenStruct.flag_authCmdGotoCHG, FSMStruct.flag_initGotoCHG and does not change it, why does it have such an effect? 

   

void Check_AuthCmdToCHG(void)
{
 if(sysInfoStruct.statusCharger == STD_FALSE)
 {
 if(pinStatus_present == STD_ON)
 {
 if(sysInfoStruct.chargerOnline == 0x1234)
 {
 sysInfoStruct.statusCharger = STD_TRUE;
 CANOpenStruct.flag_authCmdGotoCHG = STD_TRUE;
 CANOpenStruct.sendTPDOInfo= STD_TRUE; //if true,it will enable CAN TPDO
 }
 }
 else
 {
 sysInfoStruct.chargerOnline = 0;
 }
 }
}
void CheckFlag_InitGotoCHG(void)
{
 if(pinStatus_present == STD_ON)
 {
 if(CANOpenStruct.flag_authCmdGotoCHG == STD_TRUE)
 {
 CANOpenStruct.flag_authCmdGotoCHG = STD_FALSE;
 FSMStruct.flag_initGotoCHG = STD_TRUE;
 }
 }
}
uint32 Test_CANCmd(union_64bits cmd)
{
 //..........
 switch(cmd.byte[2])
 {
 case 0xF1:
 //......
 break;
 case 0xF5: //ESD Pres pin onoff times test
 if(cmd.byte[3] == 0xFF)
 {
 errCode = CANOpenStruct.flag_authCmdGotoCHG;
 }
 else if(cmd.byte[3] == 0xFE)
 {
 errCode = FSMStruct.flag_initGotoCHG;
 }
 else
 {
 errCode = TEC_cmdParaErr;
 }
 break;
 //..........
 }
 return errCode;
}

 

This topic has been closed for replies.
kevinKangBest answer
Associate
November 18, 2024

My problem has been solved!
Root cause: STM32G0B1CC is based on Arm Cortex -M0+ core, it no support unaligned accesses, pay attention to the large structure in your code.

3 replies

Visitor II
November 8, 2024

If you have debugging enabled, print the values of flag_authCmdGotoCHG, sendTPDOInfo, and FSMStruct.flag_initGotoCHG right after setting and reading them to observe any anomalies.

kevinKangAuthor
Associate
November 11, 2024

Hi liaifat85,

  Thanks for your feedback!

  My current APP code is address offset because the system comes with a bootloader. I have tried to modify the offset address and directly run online simulation, and the program works normally.

  I have tried the following 2 situations:

  S1:  

  Comment out the code for CANOpenStruct.flag_authCmdGotoCHG and FSMStruct.flag_initGotoCHG , without changing anything else, and the program works abnormally.

uint32 Test_CANCmd(union_64bits cmd)
{
 //..........
 switch(cmd.byte[2])
 {
 case 0xF1:
 //......
 break;
 case 0xF5: //ESD Pres pin onoff times test
 /*
 if(cmd.byte[3] == 0xFF)
 {
 errCode = CANOpenStruct.flag_authCmdGotoCHG;
 }
 else if(cmd.byte[3] == 0xFE)
 {
 errCode = FSMStruct.flag_initGotoCHG;
 }
 else
 {
 errCode = TEC_cmdParaErr;
 }
 */
 break;
 //..........
 }
 return errCode;
}

 S2:

  Keep CANOpenStruct.flag_authCmdGotoCHG and FSMStruct.flag_initGotoCHG code, do not change other codes, the program works fine.

kevinKangAuthorBest answer
Associate
November 18, 2024

My problem has been solved!
Root cause: STM32G0B1CC is based on Arm Cortex -M0+ core, it no support unaligned accesses, pay attention to the large structure in your code.