Skip to main content
herbert
Associate III
April 16, 2020
Question

Strange bug when updating Cube IDE on Mac to 1.3.1

When I update Cube IDE on my Mac to 1.3.1 using the built in updater, it first seems to work fine, although it keeps displaying V1.3.0. I can continue with my work, but when I leave Cube IDE and launch it again, it crashes, reporting it cannot find some Java main class.

This behaviour could not be seen on a PC, where it repeatedly works fine after updating, also correctly claiming to be V1.3.1

Has anyone else observed such a behaviour?

Regards

Herbert

This topic has been closed for replies.

6 replies

O. Mz. - 7
Associate
April 16, 2020

I updated today to STM32CubeIDE to 1.3.1 via updater on MacOS Cataline 10.15.4. Everything went well. The IDE works fine.

If you cannot find other solution try to upgrade STM32CubeMX, if necessary (or just uninstall it), and reinstall STM32CubeIDE. Though I am not sure if there is a connection between them in this context. It is just a guess.

herbert
herbertAuthor
Associate III
April 17, 2020

I use MacOS Sierra, as my Mac is a little older and cannot utilise Catalina. I have already tried reinstallation a couple of times, that did not work out. Maybe I have to wait until 1.3.1 is incorporated into the regular download (this currently only gives you 1.3.0. and you have to upgrade afterwards).

Cartu38 OpenDev
Graduate II
April 17, 2020

About version reported in startup splash screen such is only updated after an application stop and start. Eclipse restart is not sufficient. Eclipse known behavior here.​

herbert
herbertAuthor
Associate III
April 17, 2020

Yes, but the version number display is not the real problem. The real problem is that Cube IDE crashes after application restart.

mattias norlander
ST Technical Moderator
April 22, 2020

Hi Herbert,

Unfortunately there is no full installer for 1.3.1. When it comes to minor releases, we only distribute P2 updates to save bandwidth and focus our resources on more value-adding development. The only thing that changed between 1.3.0 and 1.3.1 is that the integrated MX version was stepped up from 5.6.0 to 5.6.1. MX 5.6.1 only contains two bug fixes. One related to MPU and one generic:

https://www.st.com/resource/en/release_note/dm00107607-stm32cubemx-release-561-stmicroelectronics.pdf

Hopefully you don't need the bug fixes in 1.3.1 and and you can just re-install a working full 1.3.0.

The next planned release is not a minor and will come with full installer.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
herbert
herbertAuthor
Associate III
April 22, 2020

Hello Mattias,

thanks for the info. Yes, 1.3.0 works fine for me, no problem. I am doing extended tests with CubeIDE currently as I plan a full scale transit with my university courses from Keil to CubeIDE this fall and want to make sure that my students will not experience any unpleasant surprises.

best regards

Herbert