Hello @Piotr Romaniuk ,
It is mandatory to have Chronium since ST started to use and require myST login procedure.
Some company policy allowed only EDGE and FIREFOX as web browsers so that users cannot log to their account. By installing Chromium and removing the blocking everything works as expected.
For more details, I suggest that you take a look at this Post.
- STM32CubeIDE is supported on Linux®: Ubuntu® LTS 20.04 and LTS 22.04, and Fedora® 37.
- STM32CubeMX is supported on Windows® 10 and 11, 64 bits. You can work with it offline by downloading the firmware and loading it manually. You are able also to choose the firmware package version under [Project Manager] by unchecking [Use Default Firmware Package].
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.