Skip to main content
Associate
August 17, 2023
Solved

Stm32wle5jci6

I have been working in Stm32wle5jci6,im trying to integrate My I2C code with lorawan code package downloaded from github. I had tested with Macros in that case the data was pushed in Chripstack, but whenever i try to connect the sensor i am unable to read the sensor data. Note : im using HTU31D sensor and its working. 

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
August 18, 2023

Hello @Nani96 ,

Did you manage to get a communication with your board?

When you debug your project, where the code hangs/stop?

Maybe need check your device configuration.

It will be better to attach your code and error message, this will help community users to help you.

 Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

Imen.DBest answer
ST Technical Moderator
August 18, 2023

Hello @Nani96 ,

Did you manage to get a communication with your board?

When you debug your project, where the code hangs/stop?

Maybe need check your device configuration.

It will be better to attach your code and error message, this will help community users to help you.

 Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Nani96Author
Associate
November 8, 2023

static void SendTxData(void)

{

uint16_t pressure = 0;

int16_t temperature = 0;

sensor_t sensor_data;

UTIL_TIMER_Time_t nextTxIn = 0;

 

#ifdef CAYENNE_LPP

uint8_t channel = 0;

#else

uint16_t humidity = 0;

uint32_t i = 0;

int32_t latitude = 0;

int32_t longitude = 0;

uint16_t altitudeGps = 0;

#endif /* CAYENNE_LPP */

 

// EnvSensors_Read(&sensor_data);

temperature = (SYS_GetTemperatureLevel() >> 8);

pressure = (uint16_t)(sensor_data.pressure * 100 / 10); /* in hPa / 10 */

float Temp = Get_temperature(); // function reads temperature from sensor

AppData.Port = LORAWAN_USER_APP_PORT;

 

#ifdef CAYENNE_LPP

CayenneLppReset();

CayenneLppAddBarometricPressure(channel++, pressure);

CayenneLppAddTemperature(channel++, temperature);

CayenneLppAddRelativeHumidity(channel++, (uint16_t)(sensor_data.humidity));

 

if ((LmHandlerParams.ActiveRegion != LORAMAC_REGION_US915) && (LmHandlerParams.ActiveRegion != LORAMAC_REGION_AU915)

&& (LmHandlerParams.ActiveRegion != LORAMAC_REGION_AS923))

{

CayenneLppAddDigitalInput(channel++, GetBatteryLevel());

CayenneLppAddDigitalOutput(channel++, AppLedStateOn);

}

 

CayenneLppCopy(AppData.Buffer);

AppData.BufferSize = CayenneLppGetSize();

#else /* not CAYENNE_LPP */

humidity = (uint16_t)(sensor_data.humidity * 10); /* in %*10 */

 

AppData.Buffer[i++] = AppLedStateOn;

AppData.Buffer[i++] = (uint8_t)((pressure >> 8) & 0xFF);

AppData.Buffer[i++] = (uint8_t)(pressure & 0xFF);

AppData.Buffer[i++] = (uint8_t)(temperature & 0xFF);

AppData.Buffer[i++] = (uint8_t)((humidity >> 8) & 0xFF);

AppData.Buffer[i++] = (uint8_t)(humidity & 0xFF);

 

if ((LmHandlerParams.ActiveRegion == LORAMAC_REGION_US915) || (LmHandlerParams.ActiveRegion == LORAMAC_REGION_AU915)

|| (LmHandlerParams.ActiveRegion == LORAMAC_REGION_AS923))

{

AppData.Buffer[i++] = 0;

AppData.Buffer[i++] = 0;

AppData.Buffer[i++] = 0;

AppData.Buffer[i++] = 0;

}

else

{

latitude = sensor_data.latitude;

longitude = sensor_data.longitude;

 

AppData.Buffer[i++] = GetBatteryLevel(); /* 1 (very low) to 254 (fully charged) */

AppData.Buffer[i++] = (uint8_t)((latitude >> 16) & 0xFF);

AppData.Buffer[i++] = (uint8_t)((latitude >> 8) & 0xFF);

AppData.Buffer[i++] = (uint8_t)(latitude & 0xFF);

AppData.Buffer[i++] = (uint8_t)((longitude >> 16) & 0xFF);

AppData.Buffer[i++] = (uint8_t)((longitude >> 8) & 0xFF);

AppData.Buffer[i++] = (uint8_t)(longitude & 0xFF);

AppData.Buffer[i++] = (uint8_t)((altitudeGps >> 8) & 0xFF);

AppData.Buffer[i++] = (uint8_t)(altitudeGps & 0xFF);

}

 

AppData.BufferSize = i;

#endif /* CAYENNE_LPP */

 

if (LORAMAC_HANDLER_SUCCESS == LmHandlerSend(&AppData, LORAWAN_DEFAULT_CONFIRMED_MSG_STATE, &nextTxIn, false))

{

APP_LOG(TS_ON, VLEVEL_L, "SEND REQUEST\r\n");

}

else if (nextTxIn > 0)

{

APP_LOG(TS_ON, VLEVEL_L, "Next Tx in : ~%d second(s)\r\n", (nextTxIn / 1000));

}

}

hi, my Get_temperature function always reads 0 if i tried to implement the sensor code in lorawan package.

can any one tell me what was the issue with the code. Im transmitting data in cayenne format.