Skip to main content
Associate
Sep 4, 2024 7:52 AM UTC
Question

STM32U575 USB CDC

Hello everyone,
I want to make a usb connection using USB_OTG_FS_DP and USB_OTG_FS_DM pins on the STM32U575 board. When I tried it with the examples found on the internet, it didn't work. When I tried the same method on the STM32F401 board, it was enough to select only USB_OTG_FS -> Device Only and Middleware -> USB_DEVICE -> virtual com port. What basic settings do I need to make to see my STM32U575 board as a virtual com port on the computer? I'm not very experienced in this. Thank you in advance for your help. Also, when I use the ux_device_cdc_acm example in CubeIDE, it does not appear as a virtual com port.

    This topic has been closed for replies.

    4 replies

    ST Technical Moderator
    Sep 4, 2024 9:39 AM UTC

    Hello @beenwew ,

    Ensure that the correct driver is installed and verify that the heap and stack sizes are sufficient. 

    Did you try the USB CDC example within STM32U5 firmware?

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    beenwewAuthor
    Associate
    Sep 4, 2024 10:09 AM UTC

    Yes, I tried the ux_device_cdc_acm example for the nucleo u575zi in the cube ide application. All I did was debug and plug in the usb type c cable and upload this example to the card.

     

    Associate
    Sep 3, 2025 3:37 PM UTC

    I use AZRTOS with USBX on stm32L562 for composite USB and i have this same problem - @beenwew  do you resolve problem ? debug stay in this same place on:

    B __tx_wait_here // Wait for the PendSV to happen