Skip to main content
Visitor II
Mar 19, 2025 3:35 PM UTC
Question

STM32U073/083 I2C4, not visible in SFR view

Hi

I'm using the stm32u073, the i2c4 peripheral registers are not visible in the SFR view when debugging, and the peripheral address is not included in the reference manual table 4.

I checked the .svd for u83, is the same.

Cheers

 

 

This topic has been closed for replies.

2 replies

STTwo-32
ST Technical Moderator
Mar 19, 2025 5:10 PM UTC

Salut @max34000 and welcome to the ST Community.

Thank you for escalating those typos (for the RM and the SVD file). I've escalated for correction on the coming release (under internal ticket number 205854).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Kevlar700
Associate II
Mar 24, 2025 12:15 PM UTC

The I2C4 peripheral is missing from the STM32U073.svd file. Probably missed because it isn't available on the whole stm32u0 line.