Skip to main content
Associate
Sep 12, 2026 7:41 AM UTC
Solved

STM32U031/U073/U083 SVDs incorrectly specify nvicPrioBits=4 instead of 2

The official STM32U0 SVD version 1.0 files for STM32U031, STM32U073, and
STM32U083 specify:

  <nvicPrioBits>4</nvicPrioBits>

The manual (RM0503) documents four programmable interrupt priority levels implemented with
two priority bits. ST's own current CMSIS device headers also specify the
correct value:

  stm32u031xx.h: #define __NVIC_PRIO_BITS 2
  stm32u073xx.h: #define __NVIC_PRIO_BITS 2
  stm32u083xx.h: #define __NVIC_PRIO_BITS 2

The svd metadata files are used in the rust ecosystem as well as other third party tooling.
SVD code generators exposing this value to software firmware.

I’m using the rust RTIC framework along side stm32/stm32-rs crate which depend on the SVD for source of
truth configuring for various stm32 MCUs.

The issue above manifests in the following bug in that framework:
In stm32-rs/stm32-rs, svd2rust generated `NVIC_PRIO_BITS = 4` from
the ST SVD. RTIC then converted logical priorities using four bits. Logical
priorities 1, 2, 3, and 4 were written as 0xf0, 0xe0, 0xd0, and 0xc0. The
STM32U073 hardware retains only bits 7:6, so every priority read back as 0xc0.

This prevented a nominally higher-priority LPTIM wake interrupt from preempting
an RTIC software-task executing WFI (RTIC uses NVIC priorities extensively for scheduling tasks).

Overriding the generated value to 2 made the priority read back as 0x00 and allowed my LPTIM interrupt to preempt and wake up the exclusive sleep task.

Thanks very much for reading this far

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Sep 15, 2026 7:44 AM UTC

Hello ​@jakerr 

Your detailed explanation is much appreciated.

Issue has been escalated to dev team for resolution under internal ticket ID #0065798

I will keep you posted with updates.

 

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

jakerrAuthor
Associate
Sep 15, 2026 3:29 AM UTC

As a broader suggestion, it would be great if ST could eventually make the SVD, CMSIS headers, and other device metadata generated from a single canonical register/device database.

I realize ST may already have internal tooling along these lines, but discrepancies like this suggest there is still more than one source of truth somewhere in the pipeline.

Projects such as stm32-rs have accumulated a substantial set of patches correcting or normalizing the official SVDs. It might be valuable for ST to review those corrections upstream and incorporate applicable ones into its canonical device database. Ideally, SVDs and CMSIS headers for a given MCU could then be automatically generated from this one source of truth database as part of the release process.

That would benefit not only Rust, but any third-party tooling that increasingly treats the SVD as machine-readable hardware metadata.

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Sep 15, 2026 7:44 AM UTC

Hello ​@jakerr 

Your detailed explanation is much appreciated.

Issue has been escalated to dev team for resolution under internal ticket ID #0065798

I will keep you posted with updates.

 

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.