Skip to main content
Associate III
August 15, 2024
Question

STM32U0_OTA mode

  • August 15, 2024
  • 1 reply
  • 702 views
/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

#include<stdio.h>
#include<string.h>
#include<stdlib.h>
#include<stdint.h>

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
#define GETCHAR_PROTOTYPE int __io_getchar(void)

#define FLASH_PART1 0x08000000
#define FLASH_PART2 0x08020000

#define BUFFER_SIZE 15354

char rx_data[BUFFER_SIZE];

typedef void (*pFunction)(void);

int fileSize = 0;

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

UART_HandleTypeDef huart1;
UART_HandleTypeDef huart3;

/* USER CODE BEGIN PV */

PUTCHAR_PROTOTYPE
{
 HAL_UART_Transmit(&huart3, (uint8_t *)&ch, 1, HAL_MAX_DELAY);
 return ch;
}

GETCHAR_PROTOTYPE
{
 uint8_t ch = 0;
 __HAL_UART_CLEAR_OREFLAG(&huart3);
 HAL_UART_Receive(&huart3, (uint8_t *)&ch, 1, HAL_MAX_DELAY);
 return ch;
}

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_USART3_UART_Init(void);
static void MX_FLASH_Init(void);
/* USER CODE BEGIN PFP */



/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */


void Enable_Sections(void)
{

 printf("FP N-Channel Enabled.....\r\n");
 HAL_GPIO_WritePin(GPIOD, FP_NCH_Pin,GPIO_PIN_SET);
 HAL_Delay(1000);

 printf("Mic P-Channel Enabled.....\r\n");
 HAL_GPIO_WritePin(GPIOD, MIC_PCH_Pin ,GPIO_PIN_SET);
 HAL_Delay(1000);

 printf("Mic N-Channel Enbaled....\r\n");
 HAL_GPIO_WritePin(GPIOD, MIC_NCH_Pin,GPIO_PIN_SET);
 HAL_Delay(1000);

 printf("Power key enabled.....\r\n");
 HAL_GPIO_WritePin(GPIOD, PWR_KEY_Pin,GPIO_PIN_SET);
 HAL_Delay(1000);

 printf("SIM Enbaled....\r\n");
 HAL_GPIO_WritePin(GPIOD, SIM_EN_Pin, GPIO_PIN_SET);
 HAL_Delay(1000);

 printf("Power key enabled.....\r\n");
 HAL_GPIO_WritePin(GPIOD, PWR_KEY_Pin,GPIO_PIN_RESET);
 HAL_Delay(1000);

 printf("Initializing HTTP connection...\r\n");
 HAL_Delay(10000);

}

void Disable_Sections()
{
 printf("FP N-Channel disabled.....\r\n");
 HAL_GPIO_WritePin(GPIOD, FP_NCH_Pin,GPIO_PIN_RESET);
 HAL_Delay(2000);

 printf("Mic P-Channel disabled.....\r\n");
 HAL_GPIO_WritePin(GPIOD, MIC_PCH_Pin ,GPIO_PIN_RESET);
 HAL_Delay(500);

 printf("Mic N-Channel disabled....\r\n");
 HAL_GPIO_WritePin(GPIOD, MIC_NCH_Pin,GPIO_PIN_RESET);
 HAL_Delay(2000);

 printf("SIM disabaled....\r\n");
 HAL_GPIO_WritePin(GPIOD, SIM_EN_Pin, GPIO_PIN_RESET);
 HAL_Delay(500);

}

void Clear_UART_Buffer(UART_HandleTypeDef *huart)
{
 __HAL_UART_FLUSH_DRREGISTER(huart);
 while(__HAL_UART_GET_FLAG(huart, UART_FLAG_RXNE))
 {
 (void)(huart->Instance->RDR & (uint8_t)0x00FF);
 }
 __HAL_UART_CLEAR_FLAG(huart, UART_FLAG_RXNE);
 __HAL_UART_CLEAR_OREFLAG(huart);
}

void parseCmd(char *command, int delay, char *rx_data)
{
 char rxdata[BUFFER_SIZE];
 memset(rxdata, 0, sizeof(rxdata));

 HAL_UART_Transmit(&huart1, (uint8_t*)command, strlen(command), delay);

 HAL_UART_Receive(&huart1, (uint8_t*)rxdata, BUFFER_SIZE, delay);

 memcpy(rx_data, rxdata, sizeof(rxdata));

 HAL_UART_Transmit(&huart3, (uint8_t*)rxdata, sizeof(rxdata), 1000);

 Clear_UART_Buffer(&huart1);
 Clear_UART_Buffer(&huart3);
}

uint32_t WriteToFlash(uint32_t startAddress, uint8_t *data, uint32_t dataSize)
{
 printf("\n\nWriting to Flash...\r\n");

 uint32_t newAddress = startAddress;

 if(startAddress == FLASH_PART2 )
 {
 	printf("\n\nEnter\n\n");
 data +=10; // Skip the first 10 bytes
 dataSize -=10; // Reduce the size by 10 bytes
 }
 else
 {
 	printf("\n\nnew......\n\n");
 	data += 3;
 	dataSize -= 3;
 }

 // Ensure the starting address is aligned to 8 bytes
 if (startAddress % 8 != 0)
 {
 startAddress += 8 - (startAddress % 8);
 data += 8 - (startAddress % 8);
 dataSize -= 8 - (startAddress % 8);
 }

 HAL_FLASH_Unlock();
 printf("Flash unlocked.\r\n");
 HAL_Delay(100);

 // Program the user Flash area double word by double word
 for (uint32_t i = 0; i < dataSize; i += 8)
 {
 uint64_t dataToWrite = 0;

 // Copy 8 bytes of data or less if at the end of data
 if (i + 8 <= dataSize)
 {
 memcpy(&dataToWrite, data + i, 8);
 }
 else
 {
 memcpy(&dataToWrite, data + i, dataSize - i);
 }

 if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, startAddress + i, dataToWrite) != HAL_OK)
 {
 printf("Flash programming failed at address 0x%08X\r\n", startAddress + i);
 HAL_FLASH_Lock();
 return newAddress;
 }
 else
 {
 printf("Data written to address 0x%08X\r\n", startAddress + i);
 newAddress = startAddress + i;
 }

 uint64_t readBackData = *(volatile uint64_t *)(startAddress + i);
 if (readBackData != dataToWrite)
 {
 printf("Flash verification failed at address 0x%08X. Expected: 0x%016llX, Found: 0x%016llX\r\n", startAddress + i, dataToWrite, readBackData);
 HAL_FLASH_Lock();
 return;
 }
 }

 HAL_FLASH_Lock();
 printf("Flash locked.\r\n");
 printf("Writing to Flash completed successfully.\r\n");

 return newAddress;
}

void DownloadFile(void)
{
 printf("Entering Download mode...\r\n");
 HAL_Delay(5000);

 char ATcommand[512];
 const char *host = "104.237.9.39";
 char DeviceID[] = "Zenner";
 char bin[256];
 snprintf(bin, sizeof(bin), "test/%s.bin", DeviceID);
 const int port = 80;

 printf("The bin : %s\r\n", bin);

 parseCmd("AT\r\n", 2000, rx_data);
 parseCmd("ATE0\r\n", 2000, rx_data);

 snprintf(ATcommand, sizeof(ATcommand), "AT+QHTTPURL=%d,80\r\n", snprintf(NULL, 0, "http://%s:%d/%s", host, port, bin));
 parseCmd(ATcommand, 10000, rx_data);

 snprintf(ATcommand, sizeof(ATcommand), "http://%s:%d/%s\r\n", host, port, bin);
 parseCmd(ATcommand, 10000, rx_data);

 parseCmd("AT+QHTTPGET=60\r\n", 10000, rx_data);

 uint32_t fileSize = 0;
 char *sizeStart = strstr(rx_data, "+QHTTPGET: 0,200,");
 if (sizeStart)
 {
 sizeStart += strlen("+QHTTPGET: 0,200,");

 if (sscanf(sizeStart, "%u", &fileSize) == 1)
 {
 printf("File size: %u bytes\r\n", fileSize);
 }
 else
 {
 printf("Failed to extract file size. Response: %s\r\n", rx_data);
 return;
 }
 }
 else
 {
 printf("Failed to find file size in response.\r\n");
 return;
 }

 uint32_t flashAddress = FLASH_PART2;
 FLASH_EraseInitTypeDef EraseInitStruct;
 uint32_t PageError = 0;
 EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
 EraseInitStruct.Page = (flashAddress - FLASH_BASE) / FLASH_PAGE_SIZE;
 EraseInitStruct.NbPages = (fileSize + FLASH_PAGE_SIZE - 1) / FLASH_PAGE_SIZE;

 if (HAL_FLASHEx_Erase(&EraseInitStruct, &PageError) != HAL_OK)
 {
 printf("Flash erase failed at page %lu. Error code: %lu\r\n", EraseInitStruct.Page, PageError);
 HAL_FLASH_Lock();
 return;
 }
 else
 {
 printf("Flash erase completed.\r\n");
 }

 uint32_t remainingSize = fileSize;
 uint32_t new_data = 1;

 while (remainingSize > 0)
 {

 	printf("\n\n\n");
 uint32_t chunkSize = (remainingSize > BUFFER_SIZE) ? BUFFER_SIZE : remainingSize;

 snprintf(ATcommand, sizeof(ATcommand), "AT+QHTTPGETEX=60,%u,%u\r\n",new_data,chunkSize);
 parseCmd(ATcommand, 10000, rx_data);

 memset(rx_data, 0, sizeof(rx_data));

 parseCmd("AT+QHTTPREAD=80\r\n",10000,rx_data);
 printf("\n\n\n");

 new_data = new_data + chunkSize-11;
 remainingSize -= chunkSize;

 if (strstr(rx_data, "+QHTTPREAD: 0") != NULL)
 {
 printf("\n\nDownload completed or no more data.\r\n");
 break;
 }
 else if (strstr(rx_data, "ERROR") != NULL)
 {
 printf("\n\nError on downloading the message.\r\n");
 break;
 }

 uint32_t newAddress = WriteToFlash(flashAddress,rx_data,chunkSize);
 flashAddress = newAddress + 1;
 memset(rx_data, 0, sizeof(rx_data));

 printf("Flash New address : 0x%08X\r\n", newAddress);
 printf("Flash address : 0x%08X\r\n", flashAddress);
 }
}


void jumpToApplication(uint32_t address)
{
 printf("Entered jump...\r\n");
 printf("Jumping to address: 0x%08X\r\n", address);
 typedef void (*pFunction)(void);

 __disable_irq();

 pFunction jumpToApp;
 SCB->VTOR = address;

 uint32_t stackPointer = *(volatile uint32_t *)address;
 printf("Setting stack pointer to: 0x%08X\r\n", stackPointer);
 // Set stack pointer
 __set_MSP(*(volatile uint32_t *)address);

 void (*appResetHandler)(void) = (void (*)(void))(*(volatile uint32_t*)(address + 4));

 // Get application entry point
 jumpToApp = (pFunction)(*(volatile uint32_t *)(address + 4));
 printf("Application entry point: 0x%08X\r\n", (uint32_t)jumpToApp);

 appResetHandler();

 printf("Enter to deint....\r\n");

 HAL_DeInit();

 // Jump to application
 jumpToApp();
}

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USART1_UART_Init();
 MX_USART3_UART_Init();
 MX_FLASH_Init();
 /* USER CODE BEGIN 2 */

 printf("Welcome to stm32.....\r\n");
 HAL_Delay(2000);


 Enable_Sections();

 DownloadFile();

 HAL_Delay(2000);

 Disable_Sections();

 jumpToApplication(FLASH_PART2);

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE2);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief FLASH Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_FLASH_Init(void)
{

 /* USER CODE BEGIN FLASH_Init 0 */

 /* USER CODE END FLASH_Init 0 */

 /* USER CODE BEGIN FLASH_Init 1 */

 /* USER CODE END FLASH_Init 1 */
 if (HAL_FLASH_Unlock() != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_FLASH_Lock() != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN FLASH_Init 2 */

 /* USER CODE END FLASH_Init 2 */

}

/**
 * @brief USART1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USART1_UART_Init(void)
{

 /* USER CODE BEGIN USART1_Init 0 */

 /* USER CODE END USART1_Init 0 */

 /* USER CODE BEGIN USART1_Init 1 */

 /* USER CODE END USART1_Init 1 */
 huart1.Instance = USART1;
 huart1.Init.BaudRate = 115200;
 huart1.Init.WordLength = UART_WORDLENGTH_8B;
 huart1.Init.StopBits = UART_STOPBITS_1;
 huart1.Init.Parity = UART_PARITY_NONE;
 huart1.Init.Mode = UART_MODE_TX_RX;
 huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart1.Init.OverSampling = UART_OVERSAMPLING_16;
 huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart1) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART1_Init 2 */

 /* USER CODE END USART1_Init 2 */

}

/**
 * @brief USART3 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USART3_UART_Init(void)
{

 /* USER CODE BEGIN USART3_Init 0 */

 /* USER CODE END USART3_Init 0 */

 /* USER CODE BEGIN USART3_Init 1 */

 /* USER CODE END USART3_Init 1 */
 huart3.Instance = USART3;
 huart3.Init.BaudRate = 115200;
 huart3.Init.WordLength = UART_WORDLENGTH_8B;
 huart3.Init.StopBits = UART_STOPBITS_1;
 huart3.Init.Parity = UART_PARITY_NONE;
 huart3.Init.Mode = UART_MODE_TX_RX;
 huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart3.Init.OverSampling = UART_OVERSAMPLING_16;
 huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart3) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART3_Init 2 */

 /* USER CODE END USART3_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOD, PWR_KEY_Pin|MIC_PCH_Pin|SIM_EN_Pin|MIC_NCH_Pin
 |FP_NCH_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pins : PWR_KEY_Pin MIC_PCH_Pin SIM_EN_Pin MIC_NCH_Pin
 FP_NCH_Pin */
 GPIO_InitStruct.Pin = PWR_KEY_Pin|MIC_PCH_Pin|SIM_EN_Pin|MIC_NCH_Pin
 |FP_NCH_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
    This topic has been closed for replies.

    1 reply

    Associate III
    August 15, 2024

    i am working on ota mode like stm32 with ec200 module, inneed to run the ota mode on stm32u083mct6 by partition the flash memory when i try to run the another firmware on partition 2 by jumping to it the firmware in partition 2 is not running when i try to reset jump parttion 1 its running , what is ths issues i am facing her