Skip to main content
Associate II
Jun 20, 2025 9:48 AM UTC
Question

STM32N6 Index Problem

Hello,

I am working on USB Device VCP project but I have problem about defines,index,etc. As you can see below that I have definition of "STM32N655xx" but I can not include "stm32n655xx.h".

BKaya_0-1750412741674.pngBKaya_1-1750412775627.png


I tried Index, Rebuild step but it did not fix. On the other hand, I am also getting this problem for other files. My code is giving hardfault because it can not acces to "HAL_PCD_MspInit" while initializing "HAL_PCD_Init".

I started getting code generate problems from .ioc file for N6 series but i will start new thread for this problem.

Edit:
I also forget to mention that CMSIS drivers outside of project folder as you can see below.

BKaya_0-1750416360701.png

I have "STM32N655xx" define inside of this projects but this folder can not acces to this symbol. If I can fix this, problem will be solved but I do not think that I have to do anything for this problem. Is this a bug?

 

Thanks for help,
Best Regards.

This topic has been closed for replies.

2 replies

Semer CHERNI
ST Employee
Jun 23, 2025 10:31 AM UTC

Hello @B.Kaya 

First let me thank you for posting.

Unfortunately, I am not able to reproduce the described behavior.

Could you provide the ioc file of the configuration? 

Can you check the symbols definition under C/C++ Build > Settings

SemerCHERNI_0-1750674651150.png

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
B.KayaAuthor
Associate II
Jun 23, 2025 10:34 AM UTC

Hi @Semer CHERNI ,

You can find ioc file in this thread. https://community.st.com/t5/stm32-mcus-products/usb-device-cdc-acm/m-p/815113#M281355 

BKaya_0-1750674855210.png