Skip to main content
Sid Price
Associate III
October 3, 2020
Question

STM32L524 SDMMC error reported incorrect

If a timeout occurs from "SDMMC_CmdOpCondition" (error #4) the calling function, "MMC_PowerON", returns "HAL_MMC_ERROR_UNSUPPORTED_FEATURE".

Is this correct?

Sid

This topic has been closed for replies.

6 replies

CNhan.1
Visitor II
September 12, 2021

I had the same issue as you, I don't understand why there is no suggestion from ST for this topic yet.

​

Tesla DeLorean
Guru
September 12, 2021

That's how forums often work, ST doesn't have a heavy presence here, and you're reliant of others with the same combination of hardware or ability to debug/diagnose.

Might be card specific, or a board related.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MTriv.1
Associate
December 20, 2021

I have the same issue in STM32L476G when trying an eMMC connected via microSD to eMMC adapter. Were you able to find a fix for this problem?

Rtomy.1
Associate II
September 23, 2022

Did anyone solved this? I am having the same issue in my custom board.

jerry_sandc
Associate III
November 14, 2023

I have same error occuring in the initialization code on my STM32F769-EVAL board!  :thinking_face:

I do have the SD card that came with the eval board plugged in properly.  Maybe there's some jumper setting, i'll check it out.

jerry_sandc
Associate III
November 14, 2023

I just looked at the eval board manual.  Looks like I have to make some solder modification and change a jumper to allow the SD cards to work, since some pins are shared with the camera.  You might have the same issue.