Skip to main content
Kt.11
Visitor II
March 14, 2021
Question

stm32L476G-DISCO upload not working

I have a stm32L476G-DISCO.

trying to get this simple blink led program working.

CODE:

 while (1)
 {
	HAL_GPIO_TogglePin( LD_G_GPIO_Port, LD_G_Pin );
	//(LD_R_Pin);
 HAL_Delay(2000);
 /* USER CODE END WHILE */
 MX_USB_HOST_Process();
 
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */

BUILD SUCCESS:

14:08:04 **** Incremental Build of configuration Debug for project Lab2-Kava ****
make -j8 all 
arm-none-eabi-size Lab2-Kava.elf 
 text	 data	 bss	 dec	 hex	filename
 39640	 152	 4064	 43856	 ab50	Lab2-Kava.elf
Finished building: default.size.stdout
 
 
14:08:05 Build Finished. 0 errors, 0 warnings. (took 396ms)

UPLOAD ATTEMPT:

STMicroelectronics ST-LINK GDB server. Version 5.7.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
 Persistent Mode : Disabled
 Logging Level : 1
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Disabled
 SWD Debug : Enabled
 InitWhile : Enabled
 
Waiting for debugger connection...
Debugger connected
Debugger connection lost.
Shutting down...

Really baffled why its not uploading. ST made me upload the firmware on the board.

This topic has been closed for replies.

1 reply

ChahinezC
Associate II
March 15, 2021

Hello @Kt.1​,

Welcome to ST community :smiling_face_with_smiling_eyes:.

This a debugger problem. Please check the cable you are using and make sure that you have correctly configured the Debug Configuration and connected to the ST-Link on the board.

If you are using STM32CubeIDE, I recommend you checking the 3rd section of the STM32CubeIDE User Guide.

Chahinez.