STM32L0 OTA failure
Hi ST experts,
I am using the AT command code from ST on the B-L072Z-LRWAN1. I have loaded the bin into the B-L072Z-LRWAN1 via ST-LINK3 switch on the RS232 @ 9600 and get the terminal screen with the AT command working very well.
I have a KERLINK gateway which works with the thingpark server
https://community.thingpark.io
The gateway with the EUI number shows it is connected on the server.
I can send an ABP connect and message very easily using the AT commands
However, I cannot join and send message using the OTAA mode which will complete this project.
The freq used is AS923 and I have tried all sub-bands and put the TX at MAX power.
I am using STM32CUBE IDE
This is the code path from the ST projects file when downloaded the recommended STM32CubeExpansion.
\STM32CubeExpansion_LRWAN_V2.1.0\Projects\B-L072Z-LRWAN1\Applications\LoRaWAN\LoRaWAN_AT_Slave\STM32CubeIDE\cmwx1zzabz_0xx
Please advise if there any error on the steps . Thank you.