Skip to main content
Visitor II
Apr 24, 2025 5:58 AM UTC
Question

STM32H7S78-DK - Error: failed to erase memory

I am using STM32CubeIDE to program my board i.e. STM32H7S78-DK. My file size is in large due to which it is flashing in external flash at address 0x70000000. In case of smaller file size i.e. less than 64 KB, it flashes in internal flash at address 0x08000000. The flashing was working fine in internal as well as external flash. But, all of a sudden, I am getting below error log.

-------------------------------------------------

STMicroelectronics ST-LINK GDB server. Version 7.10.0

Copyright (c) 2025, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : Enabled

 

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

-------------------------------------------------------------------

STM32CubeProgrammer v2.19.0

-------------------------------------------------------------------

 

 

 

Log output file: C:\Users\<Username>\AppData\Local\Temp\STM32CubeProgrammer_a40504.log

ST-LINK SN : 0046001A3033511935393935

ST-LINK FW : V3J16M7

Board : STM32H7S78-DK

Voltage : 3.28V

SWD freq : 8000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID : 0x485

Revision ID : Rev Y

Device name : STM32H7RSxx

Flash size : 64 KBytes (default)

Device type : MCU

Device CPU : Cortex-M7

BL Version : 0xE3

 

Opening and parsing file: ST-LINK_GDB_server_a40504.srec

 

 

Memory Programming ...

File : ST-LINK_GDB_server_a40504.srec

Size : 53.59 MB

Address : 0x70000000

 

 

 

Erasing memory corresponding to sector 0:

Erasing external memory sectors [0 7]

Error: failed to erase memory

 

 

Error: failed to erase memory

Encountered Error when opening C:\ST\STM32CubeIDE_1.18.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.100.202412061334\tools\bin\STM32_Programmer_CLI.exe

Error in STM32CubeProgrammer

Shutting down...

Exit.

-----------------------------------

Screenshot attached. Kindly help me with this issue. 

This topic has been closed for replies.

1 reply

R_1
Associate II
Apr 25, 2025 6:19 PM UTC

I just ran into a similar problem myself.
I was able to get external flash erasing to work again using the following procedure.

  • I moved SW1 to the 'BOOT0' position.
  • After power cycling the board, I was able to successfully erase/flash the external memory again using a TouchGFXDesigner example.
  • I then set SW1 back to the default position.
  • I then connected to the board in CubeProgrammer via ST-LINK in Power Down mode with hardware reset.
  • After power cycling again, the TouchGFX app was running properly.

I hope this helps!