STM32H7B3I-DK - unable to flash code to board and enter debug mode
I am using 1.10.0 STM CUBE IDE. Everything was working fine until I unchecked the box to update STLINK firmware. Now it does not work. I later updated the firmware , but still not a thing changed. This is the message I get when I try to debug console:
STMicroelectronics ST-LINK GDB server. Version 7.0.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
Error in final launch sequence:
Failed to execute MI command:
target remote localhost:61234
Error message from debugger back end:
localhost:61234: Connection timed out.
Failed to execute MI command:
target remote localhost:61234
Error message from debugger back end:
localhost:61234: Connection timed out.
localhost:61234: Connection timed out.
I tried restarting a PC it did not help. Please help I need to finish my project.