Skip to main content
Ayoub Cheggari
Senior
Apr 3, 2026 1:56 PM UTC
Solved

[STM32H750ZB][FMC] FMC_NBL0 and FMC_NBL1 are not considered in CubeIDE1.19.0

Hello,

I am using STM32H750ZB variant for an HMI custom project and I am using SDRAM via FMC.

When I configure FMC in cubeide1.19.0, I can't see the FMC_NBL0 and FMC_NBL1.

FMC.png

I can actually add these pins as GPIOs, but I can't define the AF as AF12_FMC.

I know from the datasheet that this package supports it but I want your confirmation as I still don't have HW to test and don't want to change the package again and redo the HW.

Thanks,

Ayoub 

 

Ayoub Cheggari
Ayoub CheggariBest answer
Senior
Apr 3, 2026 2:25 PM UTC

It was my mistake! I didn't check the 16_bit byte enable option!

 

image.png

4 replies

mƎALLEm
ST Technical Moderator
Apr 3, 2026 2:06 PM UTC

Hello,

1- The latest version of CubeIDE is 2.1.1. Meanwhile, starting from Cubeide 2.0.0 it's no more possible to configure your application starting from CubeIDE but rather to start it from CubeMx: please read this article: STM32CubeIDE 2.0.0 workflow tutorial

2- So you need to verify the behavior on the latest version of CubeMx.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Ayoub Cheggari
Senior
Apr 3, 2026 2:07 PM UTC

I'll try it in the latest version and let you know if I face the same issue!

Andrew Neil
Super User
Apr 3, 2026 2:07 PM UTC

@Ayoub Cheggari wrote:

cubeide1.19.0


Note that the current version is 2.1.1 - so you're a bit out-of-date.

Note also that, from v2.0.0, CubeMX is now entirely separate - it is no longer included within CubeIDE:

STM32CubeIDE 2.0.0 New workflow tutorial

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Ayoub Cheggari
Ayoub CheggariAuthorBest answer
Senior
Apr 3, 2026 2:25 PM UTC

It was my mistake! I didn't check the 16_bit byte enable option!

 

image.png