Skip to main content
Associate III
Oct 27, 2025 10:22 AM UTC
Question

stm32h7: M7 core resets OK; M4 core stuck in reset handler

Hi, im using stm32h745bit6 MCU, when im pressing reset button only M7 core is reseting and M4 core is stucking in an reset handler itself, what to do an reset. since if a use system reset also same only.

can u someone suggest what to do for this reset handler issues.

 

 

regards,

srinath

This topic has been closed for replies.

5 replies

mƎALLEm
ST Technical Moderator
Oct 27, 2025 11:02 AM UTC

Hello,

It's hard to help you based on the description you provided.

What board are you using? What example are you testing?

Please review How to write your question to maximize your chances to find a solution 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate III
Oct 27, 2025 11:08 AM UTC

Hi @mƎALLEm 

stm32h45bit3 208 pin package board we designed, in this normally i have verified peripherals, clocks, etc. during testing when i try to reset the board by push button i can see m7 core resets fine no issues, while m4 core stuck in reset handler.

thus im using an nucleo board as an debugger , so reset button is pressed in nucleo board, from here via swd connector it will go to mcu respective nrst pin.

so i couldnt able to get why it is happening like this, this first time working in an dual core.

 

 

regards,

srinath

mƎALLEm
ST Technical Moderator
Oct 27, 2025 11:12 AM UTC

Still not answering all the questions: what is the example are you using for this test?

Did you test the same thing on Nucleo board and it's working?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.