Skip to main content
AraceliGuerrero
Associate II
May 12, 2026 7:19 PM UTC
Question

STM32H7 Dual-Core Debugging: CM4 and CM7 Entry Points overlapping in CubeIDE v2.0.0

Hi everyone,

I'm experiencing a frustrating issue while debugging an STM32H755 using STM32CubeIDE v2.0.0.

When I launch a Launch Group (or start the debug sessions sequentially), the start point (Entry Point) in main often points to the exact same memory address for both the Cortex-M4 and Cortex-M7 cores (e.g., 0x81013be). This overlap obviously prevents a proper debug session.

This behavior seems random. Sometimes it starts correctly, but as I develop and recompile the code, they suddenly end up "stacked" on the same address.

Current Setup:

  • IDE: STM32CubeIDE v2.0.0.

  • GDB Server: Manually configured with separate ports (61234 and 61240).

  • Guidelines: I've followed the official dual-core debugging recommendations.

Is there a specific configuration or "hidden" setting to prevent the IDE from overlapping these entry points? Or is this a known bug in v2.0.0? It’s becoming quite a bottleneck for my development.

Thanks in advance!

 

Overlapping.png