Skip to main content
Associate
July 5, 2024
Question

STM32H563 Makefile Project breakpoint failed to stop

Hi,

Currently I don't know why my cube ide could not stop at some breakpoints that I set on the IDE.

About my project, I imported a makefile project on Cube IDE, then I set up the build and debug configuration, all the things work except the break points that are set was somehow never stopped.

I am 100% sure that the program run over the command (in this case a string was printed on a console).

The disable all breakpoint option is also disabled.

The program run normally, it also stopped at main at the beginning.

I could hit the pause button and the FW stopped at certain command.

My optimization cas currently -O0.  I also able to debug/set breakpoint under vscode (WSL) and eclipse (VM Machine). But these two are somewhat limited for my personal PC.

I also try to install extension of eclipse (Embedded JLink...), but this option is then fixed to use gdb instead of arm-none-eabi-gdb.

 

What could be the potential problem? What option should I check so that the cube IDE works just like eclipse?

By the way, the Stm32cube Programmer (2.17.0) does not seem to work on the cortex M33 (STM32H563) with Jlink yet. is there a workaround for that?

Thanks

This topic has been closed for replies.

2 replies

Roger SHIVELY
ST Employee
July 8, 2024

Hello @Khoa ,

This post has been escalated to the ST Online Support Team for additional assistance. 

We'll contact you directly.

Regards,

Roger

Visitor II
November 14, 2024

Hello, I have the same issue. I also have a makefile project which I imported into Cube IDE. I set up debug and run configurations and everything works except that execution does not stop at breakpoints. Program runs normally and I am able to pause the program. I'm using an ST Link with SWD. What is the solution?