Skip to main content
RAnge.1
Visitor II
Jan 29, 2021 9:16 AM UTC
Solved

STM32G473 DAC3 to OPAMP output stuck at low.

I'm trying to generate a signal from DAC3 (connected only to internal peripherals) from my G473 and output that value through OPAMP1 in follower mode. The output of the pin of the OPAMP is stuck at low forever however. I set the DAC from CUBEIDE as such:

static void MX_DAC3_Init(void)
 
{
 DAC_ChannelConfTypeDef sConfig = {0};
 hdac3.Instance = DAC3;
 if (HAL_DAC_Init(&hdac3) != HAL_OK) {
 Error_Handler();
 }
 
 /** DAC channel OUT1 config
 */
 sConfig.DAC_HighFrequency = DAC_HIGH_FREQUENCY_INTERFACE_MODE_AUTOMATIC;
 sConfig.DAC_DMADoubleDataMode = DISABLE;
 sConfig.DAC_SignedFormat = DISABLE;
 sConfig.DAC_SampleAndHold = DAC_SAMPLEANDHOLD_DISABLE;
 sConfig.DAC_Trigger = DAC_TRIGGER_NONE;
 sConfig.DAC_Trigger2 = DAC_TRIGGER_NONE;
 sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_DISABLE;
 sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_INTERNAL;
 sConfig.DAC_UserTrimming = DAC_TRIMMING_FACTORY;
 if (HAL_DAC_ConfigChannel(&hdac3, &sConfig, DAC_CHANNEL_1) != HAL_OK){
 Error_Handler();
 }
}

I set the OPAMP from CUBEIDE as such:

static void MX_OPAMP1_Init(void){
 hopamp1.Instance = OPAMP1;
 hopamp1.Init.PowerMode = OPAMP_POWERMODE_NORMAL;
 hopamp1.Init.Mode = OPAMP_FOLLOWER_MODE;
 hopamp1.Init.NonInvertingInput = OPAMP_NONINVERTINGINPUT_DAC;
 hopamp1.Init.InternalOutput = DISABLE;
 hopamp1.Init.TimerControlledMuxmode = OPAMP_TIMERCONTROLLEDMUXMODE_DISABLE;
 hopamp1.Init.UserTrimming = OPAMP_TRIMMING_FACTORY;
 if (HAL_OPAMP_Init(&hopamp1) != HAL_OK)
 {
 Error_Handler();
 }
}

And then on my main function, I enable DAC:

HAL_DAC_Start(&hdac3, DAC_CHANNEL_1);

and on the while loop, I set the value of the DAC:

 while (1)
 {
 /* USER CODE BEGIN 3 */
	 var = value * (0xfff+1)/3.3;
 
	 HAL_DAC_SetValue(&hdac3, DAC_CHANNEL_1, DAC_ALIGN_12B_R, var);
 
	 value += 0.5;
 
	 HAL_Delay(100);
 
	 if (value > 3) value = 0.2;
 }

Am I configuring something wrong. Is there an additional function I need to call to setup the OPAMP? DAC1 and DAC2 are in perfect working condition. Thank you!

This topic has been closed for replies.
Amel NASRI
Amel NASRIBest answer
ST Technical Moderator
Feb 2, 2021 9:29 AM UTC

Hi @RAnge.1​ ,

There is an example in the STM32CubeG4 package which is doing almost the same thing.

It is STM32Cube_FW_G4\Projects\STM32G474E-EVAL\Examples\OPAMP\OPAMP_InternalFollower.

You can also review the configuration in STM32CubeMX using the .ioc file provided there.

What I noted missing on the code you shared are the following:

  • the call of HAL_OPAMP_Start and HAL_OPAMP_Stop in the main loop
  • the call of HAL_DACEx_SelfCalibrate in MX_DAC3_Init
  • the call of HAL_OPAMP_SelfCalibrate in MX_OPAMP1_Init

Please check this and let me know if you succeeded to make it work.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.

1 reply

Amel NASRI
Amel NASRIBest answer
ST Technical Moderator
Feb 2, 2021 9:29 AM UTC

Hi @RAnge.1​ ,

There is an example in the STM32CubeG4 package which is doing almost the same thing.

It is STM32Cube_FW_G4\Projects\STM32G474E-EVAL\Examples\OPAMP\OPAMP_InternalFollower.

You can also review the configuration in STM32CubeMX using the .ioc file provided there.

What I noted missing on the code you shared are the following:

  • the call of HAL_OPAMP_Start and HAL_OPAMP_Stop in the main loop
  • the call of HAL_DACEx_SelfCalibrate in MX_DAC3_Init
  • the call of HAL_OPAMP_SelfCalibrate in MX_OPAMP1_Init

Please check this and let me know if you succeeded to make it work.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.