Skip to main content
BPai.1
Associate
Mar 10, 2020 8:13 AM UTC
Solved

STM32G070 PWM polarity register is changed

Hi,

I use HAL library to build code in CubeIDE. I use TIM1 channel 1 and 2 to output PWM.

Channel 2 is changed pulse value to change PWM duty. When I repeat to set up this value. Sometimes, the register CC2P will be changed. But, I don't change polarity value. Code of changing pulse value is as below:

void user_pwm_duty_ch2_setvalue(uint16_t value)
{
	TIM_OC_InitTypeDef sConfigOC;
 
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = value;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_2);
 HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_2);
}
static void MX_TIM1_Init(void)
{
 
 /* USER CODE BEGIN TIM1_Init 0 */
 
 /* USER CODE END TIM1_Init 0 */
 
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};
 TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
 
 /* USER CODE BEGIN TIM1_Init 1 */
 
 /* USER CODE END TIM1_Init 1 */
 htim1.Instance = TIM1;
 htim1.Init.Prescaler = PreScaler-1;
 htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim1.Init.Period = SetPeriodARR-1;
 htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim1.Init.RepetitionCounter = 0;
 htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
 sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
 if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
 {
 Error_Handler();
 }
 sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
 sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
 sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
 sBreakDeadTimeConfig.DeadTime = 0;
 sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
 sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
 sBreakDeadTimeConfig.BreakFilter = 0;
 sBreakDeadTimeConfig.BreakAFMode = TIM_BREAK_AFMODE_INPUT;
 sBreakDeadTimeConfig.Break2State = TIM_BREAK2_DISABLE;
 sBreakDeadTimeConfig.Break2Polarity = TIM_BREAK2POLARITY_HIGH;
 sBreakDeadTimeConfig.Break2Filter = 0;
 sBreakDeadTimeConfig.Break2AFMode = TIM_BREAK_AFMODE_INPUT;
 sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
 if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM1_Init 2 */
 
 /* USER CODE END TIM1_Init 2 */
 HAL_TIM_MspPostInit(&htim1);
 
}

May I ask where do I set it not correctly?

Please help me.

Thank you~

This topic has been closed for replies.
Danish1
Danish1Best answer
Lead III
Mar 10, 2020 8:30 AM UTC

At a guess, it is the line TIM_OC_InitTypeDef sConfigOC;

What you are telling the C compiler to do is to reserve some space on the stack for this temporary struct variable. And because you have not followed it by "={0}" you have not told the C compiler to set it to a specific value.

Now you do set some parts of this struct with your lines e.g. sConfigOC.Pulse = value; but the remainder of this struct is left as whatever was on the stack when you called user_pwm_duty_ch2_setvalue() - even if it makes no sense at all. Sometimes this tells HAL_TIM_PWM_ConfigChannel() to alter CC2P.

My suggestion:

Try changing line 3 to TIM_OC_InitTypeDef sConfigOC = {0};

Hope this helps,

Danish

2 replies

Danish1
Danish1Best answer
Lead III
Mar 10, 2020 8:30 AM UTC

At a guess, it is the line TIM_OC_InitTypeDef sConfigOC;

What you are telling the C compiler to do is to reserve some space on the stack for this temporary struct variable. And because you have not followed it by "={0}" you have not told the C compiler to set it to a specific value.

Now you do set some parts of this struct with your lines e.g. sConfigOC.Pulse = value; but the remainder of this struct is left as whatever was on the stack when you called user_pwm_duty_ch2_setvalue() - even if it makes no sense at all. Sometimes this tells HAL_TIM_PWM_ConfigChannel() to alter CC2P.

My suggestion:

Try changing line 3 to TIM_OC_InitTypeDef sConfigOC = {0};

Hope this helps,

Danish

BPai.1
BPai.1Author
Associate
Mar 10, 2020 8:47 AM UTC

Hi Danish,

It works normally, I must reset the value before I config it in structure.

Thank you for your remind and assistance.