Skip to main content
Associate
Dec 15, 2025 9:24 AM UTC
Question

stm32fxxx_hal.h library

Hi,

So i am using STM32CubeIDE to program my STM32 card, except that when i create my project, it doesnt generate an MX file. So when i try to include the library "stm32fxxx_hal.h", it doesn't work. Why is that? And am I obliged to work with STM32CubeMX in parallel with STM32CubeIDE?

PS : I use the latest version of the software, and my card is an stm32f303RET6.

Thank you.

15 replies

ST Technical Moderator
Dec 15, 2025 9:27 AM UTC

Hello @Lin_Me ,

 

Let me thank you for posting.

I suggest that you provide your Ioc.File.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Lin_MeAuthor
Associate
Dec 15, 2025 9:33 AM UTC

Hi, 

I do not have an Ioc.file.

I use only stm32cubeide (the latest version), i just clicked on create a new project, selected my board, and started coding, creating my .c files and headers.

 

Thank you.

mƎALLEm
ST Technical Moderator
Dec 15, 2025 9:28 AM UTC

Hello @Lin_Me and welcome to the ST community,

Which CubeIDE version are you using? if CubeIDE 2.0, there is no more possibility to generate code inside as ST annonced the CubeIDE & CubeMx divorce :) STM32CubeIDE 2.0.0 released

Otherwise how did you generate you code. Please describe in step by step and what CubeMx and CubeIDE versions are you using.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Lin_MeAuthor
Associate
Dec 15, 2025 9:34 AM UTC

Hi, 

I am using the latest version of stm32cudeide. I clicked on create a new project, i selected my board and starting creating my .c files and .h files.

Thank you.

mƎALLEm
ST Technical Moderator
Dec 15, 2025 9:37 AM UTC

As I said previously,

CubeMX is no more integrated in CubeIDE. Please download CubeMx and start your project from it and generate the project there.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
AScha.3
Super User
Dec 15, 2025 9:34 AM UTC

Hi,

> I use the latest version of the software,

-> I think this tutorial should be a good point to start with the STM32CubeIDE 2.0.0.

If IDE 2.0 , then need CubeMx first, to create a project.

So my recommendation: use IDE 1.19. for now , until tutorials matching for 2.0 .

1.19 has integrated CubeMx , should work as you expect. (I also use 1.18 and 1.19 . )

If you feel a post has answered your question, please click on " Best Answer ".
Lin_MeAuthor
Associate
Dec 15, 2025 9:36 AM UTC

Hi,

I will check it. Thank you for the advice.

TDK
Dec 15, 2025 1:02 PM UTC

stm32fxxx_hal.h isn't a file name that is generated for any chip.

For stm32f303RET6 you should be including stm32f3xx_hal.h.

#include "stm32f3xx_hal.h"

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Lin_MeAuthor
Associate
Dec 15, 2025 1:04 PM UTC

I already tried it and same result : No such file or directory. :\

TDK
Dec 15, 2025 1:40 PM UTC

> I use only stm32cubeide (the latest version), i just clicked on create a new project, selected my board, and started coding, creating my .c files and headers.

You can't create an STM32 project in STM32CubeIDE alone. That was removed with the latest update.

You must download and install STM32CubeMX and use that in standalone mode. Create a project for STM32CubeIDE.

"If you feel a post has answered your question, please click ""Accept as Solution""."
TDK
Dec 15, 2025 2:24 PM UTC

Going back to v1.19.0 would allow you to create STM32 projects from within STM32CubeIDE using the bundled/embedded STM32CubeMX.

"If you feel a post has answered your question, please click ""Accept as Solution""."