Skip to main content
超哥_it
Associate
May 6, 2020
Question

STM32F4使用STM32cubeIDE输出浮点数,程�?会进入硬件错误。

勾选了设置中的输入输出浮点,�?然无效。修改为标准库或者精简库也无效。网上也有很多人�?�到了这样的问题。请问怎么解决?官方有解决方案�?�?官方是�?�会在�?�期的版本中解决掉这个问题?

This topic has been closed for replies.

4 replies

ST Technical Moderator
May 10, 2020

Hello,

Please ask your question in English.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
超哥_it
超哥_itAuthor
Associate
May 11, 2020

Stm32f4 uses stm32code ide to output floating-point numbers, and the program will enter a hardware error.

Setting the input and output floating-point options is also invalid. Changing to a standard or thin library is also not valid. There are also many people on the Internet who have encountered such problems. How can I solve it? Is there an official solution? Will the official fix the problem in a later version?

waclawek.jan
Super User
May 11, 2020
超哥_it
超哥_itAuthor
Associate
May 13, 2020

All methods have tried or can't print floating-point numbers