Question
STM32F446RE - Disable PA0 (Reset Button) to run the code
Hi,
I'm currently using the STM32F446RE with the STM32CubeIDE. My problem at this moment is, after flashing the code it only runs when I debug through CubeIDE, but if I connect the USB it is necessary that the B2 (PA0) is pressed for the code to start running.
My question is, how can I disable this so that whenever my board receives power the code starts running without the need for the button to be pressed?
Thank you!