Associate II
June 25, 2020
Question
STM32F429I Add emWin
- 3 replies
- 847 views
Dear, I have the demo board STM32F4-discovery MB1075C
Use new STM32CubeIDE 1.3.0
Now I start a new project with this board, i need to add the emWin libray.
I have configurated the link to library and copy the file from STM32Cube_FW_F4_V1.25.0
When add the call GUI_Init(); i have this error at linking time:
GUI_Core.c:(.text.GUI__Config+0x62): undefined reference to `GUI_X_Config'
GUI_Core.c:(.text.GUI__Config+0x66): undefined reference to `LCD_X_Config'
Add the project file
Is the first time that i use the emwin
Thanks for help