Skip to main content
TOpre.1587
Visitor II
November 25, 2019
Question

STM32F429 Discovery CUBE IDE SWV printf not working

I'm using STM32F429 Discovery board and CUBE IDE. I have set the Serial Wire Debug, in debug configuration, I enabled SWV, set the core clock, enabled live expession. In main.c I wrote this part of the code

int _write(int file, char *ptr, int len)

{

   int i=0;

   for(i=0; i<len; i++)

      ITM_SendChar((*ptr++));

   return len;

}

and put some "printf" in the endless loop. In Serial Wire Viewer settings, ITM Stimulus Ports I enabled port 0, and pressed the Start Trace button. But when I started program nothing happened in the SWV ITM Data Console, it stayed blank.

I tried the same thing with the STM32F103C8 and it didn't work either. Then I tried it with STM32L476 Nucleo and with STM32H743 Nucleo, and it worked fine.

Can someone explain it to me why it doesn't work on the F4 and F1?

This topic has been closed for replies.