Skip to main content
ERena.1
Associate
November 10, 2021
Solved

STM32F407 crashes after RCC configuration

Hello !

I am currently working with a STM32F407VGT7 and I have troubles uploading some code in it. I did the simplest possible code with STM32CubeIDE : RCC configuration and some dummy operations in main while loop.

My problem is that after uploading code (with debug feature), starting it and pausing it a little while after (like 3 seconds or so), I got this error :

"Break at address "0x1fff36aa" with no debug information available, or outside of program code."

I have no idea what is causing this error. But seeing from STM32F407 datasheet that 0x1fff36aa is mapped in "System Memory + OPT" area, I guess this is not good...

I noticed that this bug doesn't occur if interrupts are disabled. Please find my code bellow.

Any idea of what could be causing this issue and how I could solve it ?

Thanks.

int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 /* USER CODE BEGIN 2 */
 uint32_t u32_dummy = 0;
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
// __disable_irq();
 
 while (1)
 {
 /* USER CODE END WHILE */
 
	 u32_dummy += 24 * 56;
 
	 u32_dummy -= 12;
 
 
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
 {
 Error_Handler();
 }
}

This topic has been closed for replies.
ERena.1
ERena.1Best answer
Associate
November 10, 2021

I found the issue : BOOT 0 pin is supposed to be pulled down (while it was pulled up).

2 replies

ERena.1
ERena.1AuthorBest answer
Associate
November 10, 2021

I found the issue : BOOT 0 pin is supposed to be pulled down (while it was pulled up).

ST Technical Moderator
November 10, 2021

Hello @ERena.1​ and welcome to the Community :)

Glad to know you overcame this problem, and thank you for your update.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks