Skip to main content
ONadr.1
Senior III
October 24, 2020
Question

STM32F103C8T6 problem debuging in CubeIDE

Hello,

I bought few Blue pill modules with this MCU. But I have a problem with them in CubeIDE (Eclipse) When I try debuging or write code into MCU, there is an Error (underneath) for all modules with this MCU (STM32F103C8T6, 99lKA 98, MYS 803)

I have the same modules with CPU form different series, and there is no problem here.

A try connect this "bad" modules to CubeProgrammer and there is everything OK. I can clear Flash, write code from file, read OB and so on. I use ST LINK V2 (two pieces, the same behavior)

I try to check where the problem is, but without succes. Perharps, anybody solve this problem and could help me.

Thanks.

STMicroelectronics ST-LINK GDB server. Version 5.6.0

Copyright (c) 2020, STMicroelectronics. All rights reserved.

Starting server with the following options:

       Persistent Mode           : Disabled

       Logging Level             : 1

       Listen Port Number        : 61234

       Status Refresh Delay      : 15s

       Verbose Mode              : Disabled

       SWD Debug                 : Enabled

       InitWhile                 : Enabled

Vendor = 0x3B

Error in initializing ST-LINK device.

Reason: ST-LINK: Could not verify ST device! Abort connection.

This topic has been closed for replies.

6 replies

MM..1
Super User
October 24, 2020

Maybe your devices is in stop mode, you need add to script debug stop mode

ONadr.1
ONadr.1Author
Senior III
October 24, 2020

How can I recognize it? I completely clear FLASH MCU a check every OB working and not working MCU. They were identical.

TDK
October 24, 2020

It's probably a counterfeit chip that ST-Link and/or GDB detected and decided not to communicate with.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ONadr.1
ONadr.1Author
Senior III
October 24, 2020

It is possible. But I dont understand, why ST Programer works corectly and code is ful functional after programing by ST Programmer. When I check the protocol from ST Programmer, I notice ID

 Device ID : 0x410

and gdb reported

Vendor = 0x3B

but I am not sure, that it is the same meaning.

MM..1
Super User
October 25, 2020

Erase MCU with Programmer and try start debug with empty MCU

ONadr.1
ONadr.1Author
Senior III
October 25, 2020

I try, but problem persist. I give it up, Perharps I buy few new MCU and rework them.

Thanks for yours advice.