Skip to main content
ZTodo.1
Associate
February 7, 2020
Solved

STM32F103C8T6 (BluePill) bricked after debugging with STM32CUBEIDE

  • February 7, 2020
  • 7 replies
  • 12840 views

I have recently bought 3 BluePills (STM32F103C8T6) and 1 ST-LINK V2 from ebay. I have been succesfully testing some old codes with Coocox Studio, but I decided to try out STM32CUBEIDE. Once I set up STM32CUBEIDE and built the program, I noticed that there's debugging option so I went with it. Unfortunately I wasn't able to debug the program - the chip would not be flashed successfully because the device would not be found or disconnected. I was/am receiving these messages

Error in final launch sequence:

Failed to execute MI command:

-exec-run

Error message from debugger back end:

Error creating process C:/Users/zdrav/Google Drive/STM32CUBEIDE/PWM/Debug/PWM.elf, (error 193).

Failed to execute MI command:

-exec-run

Error message from debugger back end:

Error creating process C:/Users/zdrav/Google Drive/STM32CUBEIDE/PWM/Debug/PWM.elf, (error 193).

Error creating process C:/Users/zdrav/Google Drive/STM32CUBEIDE/PWM/Debug/PWM.elf, (error 193).

I also can't run the program

Error starting process.

Cannot run program "C:\Users\zdrav\Google Drive\STM32CUBEIDE\PWM\Debug\PWM.elf": Launching failed

Cannot run program "C:\Users\zdrav\Google Drive\STM32CUBEIDE\PWM\Debug\PWM.elf": Launching failed

Cannot run program "C:\Users\zdrav\Google Drive\STM32CUBEIDE\PWM\Debug\PWM.elf": Launching failed

Now since I couldn't do anything from STM32CUBEIDE I decided to see if Coocox works. I wasn't able to burn the program to the Bluepill which previously was 'burned' with STM32CUBEIDE. I am receiving the following messages

Error: Connect failed, check config and cable connection

I was able to burn other Bluepills with Coocox which were not burned with STM32CUBEIDE, by just switching the Bluepill, but I thought I would want to give all 3 bluepills a burn with STM32CUBEIDE, now none of the chips can be burned.

What can be done now ?

This topic has been closed for replies.
Best answer by jblai.1

I did something similar - made my Blue Pill boards unresponsive after flashing and debugging with STM32CubeIDE. The reason was that in my project I had not switched on Serial Wire debugging in STM32CubeIDE under the System Core/SYS parameters. The solution was to move the 2 jumpers on the Blue Pill board from their default position (both near the USB connector) to the opposite position (both nearer the processor chip), press the reset button, and re-flash. Then move the jumpers back to their original position.

7 replies

Bob S
Super User
February 7, 2020

Use the STLink GUI or STM32CubeProgrammer software and see if they can connect to the board. I'm not very familiar with the blue pill boards other than they are pretty bare bones. A wild guess, but maybe, somehow, when programming from CubeIDE it set RDP mode to 1, which prevents debugging. Anyway, try the stand-alone programmer software and see what it shows. If RDP *IS* set to 1, you can then reset it to zero which will also erase the entire FLASH contents.

ZTodo.1
ZTodo.1Author
Associate
February 8, 2020

I have installed STM32CubeProgrammer and I can't connect the Bluepill to the stlink2, but I successfully upgraded the firmware

jblai.1
jblai.1Best answer
Associate II
April 13, 2020

I did something similar - made my Blue Pill boards unresponsive after flashing and debugging with STM32CubeIDE. The reason was that in my project I had not switched on Serial Wire debugging in STM32CubeIDE under the System Core/SYS parameters. The solution was to move the 2 jumpers on the Blue Pill board from their default position (both near the USB connector) to the opposite position (both nearer the processor chip), press the reset button, and re-flash. Then move the jumpers back to their original position.

ZTodo.1
ZTodo.1Author
Associate
July 13, 2020

I followed these steps and now it works like normal.

AJoha.6
Visitor II
May 9, 2022

I just did the same mistake as OP, resulting in bricking 4x stm32f103c8t6 / blue pills before i noticed. I just wanted to document and share my solution in case it ever happens again.

Hardware:

  • stm32f103c8t6 (1x "real" and 3x "fake")
    • Both jumper on BOOT-mode (both near usb)
    • USB-power
  • 1x ST-LINK V2-1 (From nucleon-l476rg) with updated FW (Latest ver. as of 2022-05-09)

Software:

  • STM32cube programmer (Latest ver. as of 2022-05-09)
    • Port: SWD
    • Freq.: 4000
    • Mode: Under Reset
    • Acces. port: 0
    • Reset mode: Hardware ..
    • Speed: reliable
    • Shared: Disabled
  • Debian 20.04 (Linux)

Problem:

  • The blue pills got bricked after using STM32cubeIDEs programming interface (Run debug/Run Application). It worked when i was using CLI for st-link (e.g. st-link --probe) before downloading cubeIDE.
  • Can reach the blue pill when holding down reset, but not when releasing.

Error codes:

  • Error in initializing ST-LINK device.

Reason: No device found on target.

  • Failed to enter SWD mode
  • Failed to connect to target
  • ERROR common.c: Can not connect to target. Please use 'connect under reset' and try again

Solution:

  • Set jumper from NRST (marked "R" on board) to NRST on ST-LINK V2
  • Connect with STM32CUBE programmer (set as in "Hardware")
  • Press eraser button (Erase all) -> OK
  • Confirmed by: st-link --probe -> st-flash write .... (Solution OK)

I hope this helps!

Visitor II
June 17, 2024

thach2024_0-1718628229657.pngthach2024_1-1718628234054.pngthach2024_2-1718628240038.png

thank you very much for your solution,  I am a fresher with Microcontroller programing, I have same trouble my board was blocked, I have try to solve it as your advice but it still do not connected although it can update drivers,

could you please  share some picture for me do the right way. 

 

 

 

Peter BENSCH
ST Technical Moderator
April 25, 2025

This relates to a so-called Blue Pill, which uses illegally cloned STM32F103. ST resources are only dedicated to supporting genuine ST products. We are not committed to ensuring that clones/fakes products work properly with the firmware we provide.

We recommend to purchase genuine products from STMicroelectronics and purchase them from known and trusted distributors.

This thread will now be locked. However, if you face difficulties while using genuine ST products, we’re here to assist you. Please feel free to start a new thread, and our team, along with community members, will be ready to help you with any issues/questions you encounter.

Thank you for your understanding.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.