Skip to main content
robsn
Associate
November 15, 2019
Question

[STM32F1] LL_GPIO not setting pins in CubeIDE generated MX_GPIO_Init

When I set a GPIO output level to high in the device configuration tool, it generates an LL_GPIO_SetOutputPin call on top just below the EnableClocks inside the MX_GPIO_Init function. This doesn't work. When I copy this call to the bottom of the generated function it works:

static void MX_GPIO_Init(void)
{
 LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* GPIO Ports Clock Enable */
 LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_GPIOC);
 LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_GPIOD);
 LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_GPIOA);
 LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_GPIOB);
 
 /* * * * * * * * The generated calls below do not set the GPIOs * * * * * * * */
 
 /**/
 LL_GPIO_SetOutputPin(FW_INT_NRST_GPIO_Port, FW_INT_NRST_Pin);
 
 /**/
 LL_GPIO_SetOutputPin(SER_DATA_SEL_GPIO_Port, SER_DATA_SEL_Pin);
 
 /**/
 LL_GPIO_ResetOutputPin(MCU_GPIO0_GPIO_Port, MCU_GPIO0_Pin);
 
 /* * * * * * * * The generated calls above do not set the GPIOs * * * * * * * */
 
 /**/
 GPIO_InitStruct.Pin = PGOOD_Pin;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_FLOATING;
 LL_GPIO_Init(PGOOD_GPIO_Port, &GPIO_InitStruct);
 
 /**/
 GPIO_InitStruct.Pin = LL_GPIO_PIN_14|LL_GPIO_PIN_15|LL_GPIO_PIN_0|LL_GPIO_PIN_1 
 |LL_GPIO_PIN_2|LL_GPIO_PIN_3|LL_GPIO_PIN_4|LL_GPIO_PIN_5 
 |LL_GPIO_PIN_6|LL_GPIO_PIN_7|LL_GPIO_PIN_8|LL_GPIO_PIN_9 
 |LL_GPIO_PIN_12;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
 LL_GPIO_Init(GPIOC, &GPIO_InitStruct);
 
 /**/
 GPIO_InitStruct.Pin = LL_GPIO_PIN_0|LL_GPIO_PIN_1|LL_GPIO_PIN_2|LL_GPIO_PIN_3 
 |LL_GPIO_PIN_4|LL_GPIO_PIN_5|LL_GPIO_PIN_7|LL_GPIO_PIN_8 
 |LL_GPIO_PIN_12;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
 LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 /**/
 GPIO_InitStruct.Pin = LL_GPIO_PIN_0|LL_GPIO_PIN_2|LL_GPIO_PIN_10|LL_GPIO_PIN_11 
 |LL_GPIO_PIN_12|LL_GPIO_PIN_13|LL_GPIO_PIN_14|LL_GPIO_PIN_15 
 |LL_GPIO_PIN_5|LL_GPIO_PIN_6|LL_GPIO_PIN_7|LL_GPIO_PIN_8;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
 LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 
 /**/
 GPIO_InitStruct.Pin = FW_INT_NRST_Pin|MCU_GPIO0_Pin;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT;
 GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
 LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 
 /**/
 GPIO_InitStruct.Pin = SER_DATA_SEL_Pin;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT;
 GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
 LL_GPIO_Init(SER_DATA_SEL_GPIO_Port, &GPIO_InitStruct);
 
 /**/
 GPIO_InitStruct.Pin = LL_GPIO_PIN_2;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
 LL_GPIO_Init(GPIOD, &GPIO_InitStruct);
 
 /* * * * * * * * They do work when I copy them here: * * * * * * * */
 
 /**/
 LL_GPIO_SetOutputPin(FW_INT_NRST_GPIO_Port, FW_INT_NRST_Pin);
 
 /**/
 LL_GPIO_SetOutputPin(SER_DATA_SEL_GPIO_Port, SER_DATA_SEL_Pin);
 
 /**/
 LL_GPIO_ResetOutputPin(MCU_GPIO0_GPIO_Port, MCU_GPIO0_Pin);
 
}

HW is STM32F107RCT. Is this a known issue?

This topic has been closed for replies.

4 replies

waclawek.jan
Super User
November 17, 2019

Maybe Delay after an RCC peripheral clock enabling erratum, have a look e.g. in https://www.st.com/content/ccc/resource/technical/document/errata_sheet/0a/98/58/84/86/b6/47/a2/DM00037591.pdf/files/DM00037591.pdf/jcr:content/translations/en.DM00037591.pdf . I know it's the 'F40x erratum and not 'F10x, but the latter hasn't been updated for some quite time, and the underlying principle is the same.

JW

robsn
robsnAuthor
Associate
November 18, 2019

Thank you for the answer. I tried to insert a delay between enabling the clocks and setting the output pins with LL_mDelay(1000) which of course is way too much. Didn't work. But maybe it can't be tested that way. I currently initially set them in main before the while(1) to not get overwritten by the generator.

waclawek.jan
Super User
November 18, 2019

> I tried to insert a delay between enabling the clocks and setting the output pins with LL_mDelay(1000) which of course is way too much. Didn't work.

Then maybe it's something else.

I don't use Cube and don't use the 'F1 (which are different from other STM32 when it comes to GPIO). So maybe try to have a look inside the functions you are calling, and observe the registers as you step through them.

JW

izilzty
Visitor II
December 28, 2019

Hi

I had the same problem on F103 and I solved it by setting GPIO Pull-up / Pull-down to Pull-up in CubeMX. I noticed it actually sets ODR instead of PUPDR.

Like waclawek.jan said, I also think it's a register difference.

Sorry for my bad english.