Skip to main content
Mohamed eleuche
Associate III
Dec 31, 2025 4:11 PM UTC
Solved

STM32F030 problem reading two ADC channels with DMA

Hello, I am getting really frustrated with this issue for almost a week.

I am trying to read PA1 and PA4 in DMA but I get only the reading of one channel and not the other one! I tried everything and I also looked at all the example online. Please help.

 

TDK
TDKBest answer
Dec 31, 2025 4:58 PM UTC

> I get only the reading of one channel and not the other one!

Why do you think that is the case? What readings do you get and what do you expect instead? Be specific.

> uint32_t adcValues[100]

> hdma_adc.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;

This should be an array of uint16_t, not uint32_t.

"If you feel a post has answered your question, please click ""Accept as Solution""."

4 replies

TDK
TDKBest answer
Dec 31, 2025 4:58 PM UTC

> I get only the reading of one channel and not the other one!

Why do you think that is the case? What readings do you get and what do you expect instead? Be specific.

> uint32_t adcValues[100]

> hdma_adc.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;

This should be an array of uint16_t, not uint32_t.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Mohamed eleuche
Associate III
Jan 1, 2026 4:27 PM UTC

Hello TDK,

thank you for your interest.

I think there are some mistakes in my code (that's why I shared the 3 main files). If someone can be so kind to have a look or suggest a working example to look at.

in my array I get:

adcValues[0]= 200 , 

adcValues[1]= 0  ,

adcValues[2]= 190 , 

adcValues[3]= 0  ,

adcValues[4]= 201 , 

adcValues[5]= 0  ,

and so fourth ...

 

 

 

TDK
Jan 1, 2026 5:25 PM UTC

Did you correct the error I noted?

"If you feel a post has answered your question, please click ""Accept as Solution""."