Skip to main content
dmista
Associate
Mar 13, 2025 12:52 AM UTC
Question

STM32CubeIDE X Window System error - BadRequest

Running the STM32CubeIDE v1.17.0 on Ubuntu 22.04 - exits after the splash screen.
I installed "en.st-stm32cubeide_1.17.0_23558_20241125_2245_amd64.sh.zip"

I tried searching for this issue but got nothing. What am I doing wrong?

Here the output:

$ ~/st/stm32cubeide_1.17.0/stm32cubeide
libEGL warning: DRI2: failed to authenticate

(STM32CubeIDE:101990): Gdk-ERROR **: 17:47:03.266: The program 'STM32CubeIDE' received an X Window System error.
This probably reflects a bug in the program.
The error was 'BadRequest (invalid request code or no such operation)'.
(Details: serial 2525 error_code 1 request_code 155 (unknown) minor_code 1)
(Note to programmers: normally, X errors are reported asynchronously;
that is, you will receive the error a while after causing it.
To debug your program, run it with the GDK_SYNCHRONIZE environment
variable to change this behavior. You can then get a meaningful
backtrace from your debugger if you break on the gdk_x_error() function.)

This topic has been closed for replies.