Skip to main content
Visitor II
Apr 5, 2025 6:28 PM UTC
Solved

STM32CubeIDE Warning: "This peripheral has no parameter to be configured

Hey everyone :waving_hand:,

After installing STM32CubeIDE, I encountered the following warning:

"This peripheral has no parameter to be configured"

At first, I thought it was an error — but after doing some research, I realized it's probably nothing serious.

However, to be sure, I tried everything I could:

  • Reinstalled STM32CubeIDE

  • Changed system settings

  • Updated all available packages and tools

Despite all of this, the warning still appears whenever I configure certain peripherals.

Can someone help me understand if this is normal behavior? Should I ignore it, or is there a proper way to fix or suppress this warning?

Any guidance would be greatly appreciated!

Thanks in advance!

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Apr 5, 2025 7:04 PM UTC

Hello @yashvee and welcome to the ST Community.

if you are tooking about the working in this Screenshot :

STTwo32_0-1743879614903.png

It is just added to mention that for this peripheral, there is not more parameter to be configured on the configuration window of the interface. For example, on the configuration of the USART, you will have some parameters to configure on the configuration menu.

Nothing to worry about.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Apr 5, 2025 7:04 PM UTC

Hello @yashvee and welcome to the ST Community.

if you are tooking about the working in this Screenshot :

STTwo32_0-1743879614903.png

It is just added to mention that for this peripheral, there is not more parameter to be configured on the configuration window of the interface. For example, on the configuration of the USART, you will have some parameters to configure on the configuration menu.

Nothing to worry about.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.