Skip to main content
TJM
Senior II
Feb 19, 2026 1:54 PM UTC
Solved

STM32CubeIDE v2.0 some random files are not found after migration

Upgraded to v2.  I know this is a general question and I can elaborate but I'm having issues with my project NOT finding files.  First, has there been some change in the formatting for the entries in the Include portion of the project properties, General, Paths and Symbols...?  I'm doing a project where the paths are provided in an .xml file to be imported.  Most of it works but it appears some random files are not found.  I say random because if I fix one, two or more files are not found.  There must be some formatting issue OR maybe I'm not clear of the ORDER of the includes that may make a difference.  I've gotten the errors to drop from 15 down to 2, then fixing those 2 then results in 5 more.  I'm doing something incorrectly and not recognizing the problem, most likely.  

Any suggestions would help.

Thanks,

Tony

TJM
TJMBest answer
Senior II
Mar 4, 2026 3:55 PM UTC

Thanks for the reply.  The problem is resolved but I'm not sure what caused the issue.  I tried changing, adding and removing PATH entries and found that solving one 'file not found' issue then caused another.  The issue was resolved by deleting and reloading the entire project, re-loading the paths, which were present in the form of a paths.xml file.  This project reload was actually done twice with the second time successful.  The project is embedded in an online course and I don't discount the possibility that I may have mis-read something, done something or caused some mis-step that interrupted the flow of the project.  I consider it resolved at this time.

 

Thanks,

Tony

2 replies

ST Technical Moderator
Mar 4, 2026 1:38 PM UTC

Hello @TJM 

Could you attach your project in order to investigate further the issue?

BR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
TJM
TJMAuthorBest answer
Senior II
Mar 4, 2026 3:55 PM UTC

Thanks for the reply.  The problem is resolved but I'm not sure what caused the issue.  I tried changing, adding and removing PATH entries and found that solving one 'file not found' issue then caused another.  The issue was resolved by deleting and reloading the entire project, re-loading the paths, which were present in the form of a paths.xml file.  This project reload was actually done twice with the second time successful.  The project is embedded in an online course and I don't discount the possibility that I may have mis-read something, done something or caused some mis-step that interrupted the flow of the project.  I consider it resolved at this time.

 

Thanks,

Tony