Skip to main content
Associate
Mar 25, 2026 2:14 PM UTC
Solved

stm32cubeide V 2.1.1 crtn.o executable stack bug back again despite having -z noexecstack set

Hi,

I encountered this bug with a previous update and after searching I added the -z noexecstack parameter as given in a 2025 post.

That cleared the problem at the time.

 

The IDE has updated itself to V2.1.1 and the bug has re-appeared, despite the noexecstack parameter still being present?

 

Full error:

C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.14.3.rel1.win32_1.0.100.202602081740/tools/bin/../lib/gcc/arm-none-eabi/14.3.1/../../../../arm-none-eabi/bin/ld.exe: warning: C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.14.3.rel1.win32_1.0.100.202602081740/tools/bin/../lib/gcc/arm-none-eabi/14.3.1/thumb/v7e-m+dp/hard/crtn.o: missing .note.GNU-stack section implies executable stack
C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.14.3.rel1.win32_1.0.100.202602081740/tools/bin/../lib/gcc/arm-none-eabi/14.3.1/../../../../arm-none-eabi/bin/ld.exe: NOTE: This behaviour is deprecated and will be removed in a future version of the linker

(The IDE has been updated each time it prompted since the 1.19.0 install).

A second compile with no changes after clearing the error message completes OK, but this rather tedious when working on and debugging a big project.

 

Any work-around appreciated.

 

ST Technical Moderator
Mar 27, 2026 2:05 PM UTC

Hello @rjenkinsgb 

Let me thank you for your feedback.

This is a known limitation marked on STM32CubeIDE:STM32CubeIDE errata 2.1.x - stm32mcu.

As work around, I recommend that you add this flag -z noexecstack under (Project > Properties > C/C++ Build > Settings > MCU/MPU GCC Linker > Miscellaneous > Other Flags) and the build will be finished with 0 errors.

[See Attachment]

Thanks

Mahmoud

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

ST Technical Moderator
Mar 27, 2026 2:05 PM UTC

Hello @rjenkinsgb 

Let me thank you for your feedback.

This is a known limitation marked on STM32CubeIDE:STM32CubeIDE errata 2.1.x - stm32mcu.

As work around, I recommend that you add this flag -z noexecstack under (Project > Properties > C/C++ Build > Settings > MCU/MPU GCC Linker > Miscellaneous > Other Flags) and the build will be finished with 0 errors.

[See Attachment]

Thanks

Mahmoud

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
Mar 27, 2026 2:56 PM UTC

Hi Mahmoud,

thanks for the reply.

I had previously added that flag, which is why I was confused that the error was still occurring.

 

What I did not notice until re-checking just now is that the flag settings are separate between debug and release builds, and I had only added it in one rather than both. so it re-appeared when I changed the build I was using.

 

I now have it set in both which will hopefully fix the problem for good!

 

Thanks again, Robert.