Skip to main content
Rodo
Senior
Jul 2, 2026 5:45 AM UTC
Question

STM32CubeIDE v 1.19.0 error downloading crdb.zip?

Hi all,

I know there is a newer version of this (v2.2) but I'm still on the old one. I can click the ok button on the "Download has failed, some data may be not updated. Please retry later" window and the target selector shows up but the project I make (TestH7A3VIT6) for STM32H7A3VIT6 has an exclamation point on a triangle in it.

BTW I'm using this in my windows 11 laptop and there is no crdb.zip in the repository folder.

So is STM32CubeIDE 1.19.0 too old and not supported anymore? I'm trying to avoid some of the early bugs in STM32CubeIDE v 2.x.

Thanks

 

22 replies

kaamil1984
Associate II
Aug 20, 2026 8:52 PM UTC

I think they are cutting off versions older than 2.0 :/