Skip to main content
CTabo.1
Senior
Jan 16, 2024 9:21 AM UTC
Solved

STM32CubeIDE upgrade

Hello, 
I have recently upgradated STM32CubeIDE from v.1.13.2 to v.1.14.0.

The upgrade seems has gone well, as indicated in the Help->About window:

CTabo1_1-1705396108646.png

Anyway, if i check the window installed application list, is still indicated the previous version:

CTabo1_0-1705396031665.png

Also, in the file system I continue to see the old version 1.13.2, but not the new one 1.14.0.

CTabo1_0-1705396433143.png

This doesn't seem to be very clear and I am a little bit confused.
Is it better to disinstall a reinstall STM32CubeIDE?

Regards,
Carlo

 

    This topic has been closed for replies.
    Imen.DBest answer
    ST Technical Moderator
    Jan 16, 2024 10:12 AM UTC

    Hello @CTabo.1 

    It is possible to install new versions of STM32CubeIDE in parallel with older versions.

    I recommend you follow the steps in the "UM2563: STM32CubeIDE installation guide" to update an STM32CubeIDE installation.

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

    4 replies

    Imen.DBest answer
    ST Technical Moderator
    Jan 16, 2024 10:12 AM UTC

    Hello @CTabo.1 

    It is possible to install new versions of STM32CubeIDE in parallel with older versions.

    I recommend you follow the steps in the "UM2563: STM32CubeIDE installation guide" to update an STM32CubeIDE installation.

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    CTabo.1
    CTabo.1Author
    Senior
    Jan 18, 2024 4:27 PM UTC

    Thank you @Imen.D.

    Regards,
    Carlo

    TDK
    Jan 16, 2024 2:04 PM UTC

    If the about screen says 1.14.0, I wouldn't worry about it. If on Windows, you can right click the icon and find the EXE that is running. It could be that it installed it within the v1.13.2 directory, but it could also have been placed in a local user folder.

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    Visitor II
    Sep 24, 2025 2:09 AM UTC

    I recently upgraded STM32CubeIDE from v1.13.2 to v1.14.0 and noticed something similar — the Help → About window shows the correct updated version, but in the Windows application list and filesystem the old version (1.13.2) still appears. It can be a bit confusing.

    A clean uninstall and reinstall usually clears up these mismatches and ensures only the latest version remains.
    For anyone facing such upgrade or setup issues.