Skip to main content
costi
Associate III
March 20, 2024
Solved

STM32CubeIDE update with the version 1.15.0

The last update of CubeIDE is like below:

costi_0-1710947767043.png

I have this warning and I don't understand what it is:

"C:/ST/STM32CubeIDE_1.3.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.100.202403111256/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: warning: FW_code123_R1-0.elf has a LOAD segment with RWX permissions"

 

After this CubeIDE update, the FW update is required for ST_Link/V2 Programmer

costi_1-1710948323541.png

I pressed the "Open in update mode" button.

The error bellow is present now, like bellow:

costi_2-1710948410908.png

What can I do to solve this aspect?

I can't use the programmer to program the micro controller or to make a FW debug.

Thanks in advanced

Constantin

P.S.

before of this last update, the mentioned warning was not present. I used the same FW code. And the ST_Link/V2 FW update was working every time when the CubeIDE requested for it

The ST_Link/V2 programmer is OK. I use it on the other PC and I test it also using ST_Link Utility and on this tool the FW update is working and the controller can be programmed.

    This topic has been closed for replies.
    mƎALLEm
    mƎALLEmBest answer
    ST Technical Moderator
    March 21, 2024

    Hello @costi & @gfm ,

    Try to update your ST-Link FW with the STSW-LINK007 ST-Link firmware updater application.

     

     

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

    5 replies

    Visitor II
    March 21, 2024

    Same problem.

    Trying to  flash a STM32F4 Discovery board from CubeIDE.

    mƎALLEm
    mƎALLEmBest answer
    ST Technical Moderator
    March 21, 2024

    Hello @costi & @gfm ,

    Try to update your ST-Link FW with the STSW-LINK007 ST-Link firmware updater application.

     

     

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
    Visitor II
    March 21, 2024

    Ok, it's working now. Thanks

    mƎALLEm
    ST Technical Moderator
    March 22, 2024

    Note that the proposed solution is just a workaround. The issue need to be fixed in CubeIDE.

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
    costi
    costiAuthor
    Associate III
    March 22, 2024

    For the mentioned warning follow the link below:

    https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-15-0-elf-has-a-load-segment-with-rwx-permissions/m-p/652509#M25301

    I tried that suggestion and it's working.