Skip to main content
Associate II
Dec 12, 2025 12:01 AM UTC
Solved

STM32CubeIDE terminal can't connect after very first debug-session

Hi,

still pretty, pretty new to STM32CubeIDE, I'm trying to understand how it works by doing little things. So right now I'm trying to combine both debugger with a terminal both running in STM32CubeIDE.

To include terminal in STM32CubeIDE I have followed instruction given here:

How to use the STM32CubeIDE terminal to send and receive data (Knowledge Base) 

So far, running a little test program, I was succesfull doing it at least for very first debug session (i.e. after power cycling the Nucleo-Board). I quit the debug session with the indicated button shown on attached figure below

Screenshot 2025-12-12 001635.png

However, when I start a debug session a second time, I get always(!) the same error message (see below)

Screenshot 2025-12-12 001907.png

The only way I found so far is to make a hard power cycle to the Nucleo-Board to make it connected in the STM32CubeIDE again.

Well, in STM32CubeIDE, because I also installed Tera Term and here everything is working fine. But actually I'm a fan of having thing in one application that can be in one.

So my question is: Is there a better way of connecting the terminal again in STM32CubeIDE after quitting a debug session?

Regards

Sebastian

Win11, STMCubeIDE 2.0, Nucleo-L432 Board

Below my main.h and main.c file (don't know if it helps)

  • main.h
/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.h
 * @brief : Header for main.c file.
 * This file contains the common defines of the application.
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */

/* Define to prevent recursive inclusion -------------------------------------*/
#ifndef __MAIN_H
#define __MAIN_H

#ifdef __cplusplus
extern "C" {
#endif

/* Includes ------------------------------------------------------------------*/
#include "stm32l4xx_hal.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Exported types ------------------------------------------------------------*/
/* USER CODE BEGIN ET */

/* USER CODE END ET */

/* Exported constants --------------------------------------------------------*/
/* USER CODE BEGIN EC */

/* USER CODE END EC */

/* Exported macro ------------------------------------------------------------*/
/* USER CODE BEGIN EM */

/* USER CODE END EM */

/* Exported functions prototypes ---------------------------------------------*/
void Error_Handler(void);

/* USER CODE BEGIN EFP */

/* USER CODE END EFP */

/* Private defines -----------------------------------------------------------*/
#define MCO_Pin GPIO_PIN_0
#define MCO_GPIO_Port GPIOA
#define VCP_TX_Pin GPIO_PIN_2
#define VCP_TX_GPIO_Port GPIOA
#define SWDIO_Pin GPIO_PIN_13
#define SWDIO_GPIO_Port GPIOA
#define SWCLK_Pin GPIO_PIN_14
#define SWCLK_GPIO_Port GPIOA
#define VCP_RX_Pin GPIO_PIN_15
#define VCP_RX_GPIO_Port GPIOA
#define LD3_Pin GPIO_PIN_3
#define LD3_GPIO_Port GPIOB

/* USER CODE BEGIN Private defines */

/* USER CODE END Private defines */

#ifdef __cplusplus
}
#endif

#endif /* __MAIN_H */
  • main.c
/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <stdio.h>
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart2;

/* USER CODE BEGIN PV */
uint32_t myCnt = 200;
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USART2_UART_Init();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
	/* HAL_GPIO_TogglePin(LED3_GPIO_PORT, LED3_PIN); */
	 HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_3);
	 HAL_Delay(myCnt);
	/* Loop delay time */
	 myCnt = myCnt + 100;
	 if (myCnt > 1000) myCnt = 200;
	/* Serve USART2 with Hello World	 */
	 printf("Hello World, the delay in next cycle is\t%d\n\r", (int)myCnt);

 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure LSE Drive Capability
 */
 HAL_PWR_EnableBkUpAccess();
 __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE|RCC_OSCILLATORTYPE_MSI;
 RCC_OscInitStruct.LSEState = RCC_LSE_ON;
 RCC_OscInitStruct.MSIState = RCC_MSI_ON;
 RCC_OscInitStruct.MSICalibrationValue = 0;
 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
 RCC_OscInitStruct.PLL.PLLM = 1;
 RCC_OscInitStruct.PLL.PLLN = 16;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Enable MSI Auto calibration
 */
 HAL_RCCEx_EnableMSIPLLMode();
}

/**
 * @brief USART2 Initialization Function
 * None
 * @retval None
 */
static void MX_USART2_UART_Init(void)
{

 /* USER CODE BEGIN USART2_Init 0 */

 /* USER CODE END USART2_Init 0 */

 /* USER CODE BEGIN USART2_Init 1 */

 /* USER CODE END USART2_Init 1 */
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;
 huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART2_Init 2 */

 /* USER CODE END USART2_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 /* USER CODE BEGIN MX_GPIO_Init_1 */

 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(LD3_GPIO_Port, LD3_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : LD3_Pin */
 GPIO_InitStruct.Pin = LD3_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(LD3_GPIO_Port, &GPIO_InitStruct);

 /* USER CODE BEGIN MX_GPIO_Init_2 */

 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
 /*
 * @brief Retargets the C library printf function to the USART.
 * None
 * @retval None
 */
	PUTCHAR_PROTOTYPE
	{
	 /* Place your implementation of fputc here */
	 /* e.g. write a character to the USART1 and Loop until the end of transmission */
	 HAL_UART_Transmit(&huart2, (uint8_t *)&ch, 1, 0xFFFF);
	 return ch;
	}

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

DSebastianBest answer
Associate II
Dec 15, 2025 10:24 PM UTC

ooooooooooooooooooooohhhh. I guess I found my mistake (aarrg, why the icons in STM32CubeIDE are so small) - so I had a look on the linked discription again where it was said:

"This also works while in debug mode and you can switch the “Console view” by clicking and expanding this icon"

... I thought the icons are the same. But actually the are not.

So, for the very first connection (either in editing or debug mode), one has to click on this icon (sorry for screen shots again):

Click on "3 Command Shell Console"Click on "3 Command Shell Console"

Then, once the connection is established, one need to select the console to display for any further view by clicking on the icon just left to it and select it (screen shot below).
Under 3 the connected Nucleo_L432 (name I have choosen) an be selectedUnder 3 the connected Nucleo_L432 (name I have choosen) an be selected

I leave the pictures large to see the icons in a better way.

... and now I don't know where to place the solution marker. Thanks to Andrew Neil and Pavel A!

15 replies

Andrew Neil
Super User
Dec 13, 2025 6:56 PM UTC

Can any other terminal connect to COM6 (or whatever) when the IDE is in this state?

 

I've never used the built-in terminal - I always prefer to use a standalone terminal (eg, TeraTerm)

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
Dec 15, 2025 8:33 PM UTC

@Andrew Neil wrote:

Can any other terminal connect to COM6 (or whatever) when the IDE is in this state?

No, starting TeraTerm after IDE being is not possible.

BUT, I can do the following

  1. Doing a power cycle at the nucleo board to start fresh
  2. Connect TeraTerm -> the messages a properly displayed (no surprise)
  3. Start Debug in IDE. During this, terminal on tera term is on hold (somehow expected)
  4. Open console in IDE (works)
  5. Stepping through main is fine, messages are displayed in TeraTerm
  6. Terminate debugging
  7. Start Debug IDE (see step 3 above) ... I can continue this forever

So, this effect is limited to the terminal started in IDE.

Andrew Neil
Super User
Dec 15, 2025 8:56 PM UTC

@DSebastian wrote:

@Andrew Neil wrote:

Can any other terminal connect to COM6 (or whatever) when the IDE is in this state?

No, starting (sic?) TeraTerm after IDE being is not possible.


It shouldn't affect starting TeraTerm - should just mean that TeraTerm can't open the connection?

TeraTerm should say something like:

AndrewNeil_0-1765831999504.png or AndrewNeil_2-1765832140334.png

 

and then open in 'Disconnected' mode:

AndrewNeil_1-1765832039738.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Pavel A.
Dec 13, 2025 11:54 PM UTC

The serial terminal of CubeIDE is part of the "upstream" Eclipse. If you suspect a bug (such as attempt to spawn another instance of terminal on same COM port, which won't work) - please help ST to reproduce it and report.

 

Associate II
Dec 15, 2025 9:19 PM UTC

Well, it reproducible with the steps described:

  1. Start IDE
  2. start debug
  3. Connect terminal
  4. do debugging - (fine)
  5. terminate debugging
  6. start debug
  7. terminal connection closed, only power cycle is helping

With respect to spawn another instance, this might be actually the case, because looking into details it looks like attached one can see that several instances appear (sorry for the screen shot, but drop down menus close when application is switched).

IMG_2209.jpeg

Probably one more hint/idea from my side:
When I open a new console prior to switching to debug mode, and make this new console a "Command Shell Console", then I get, hm, two consoles showing the same (see below)
Screenshot 2025-12-15 220011.png
But one of the consoles disappear when I start the debugger ... and connection is lost

Screenshot 2025-12-15 221615.png

Don't know if this is important, but for debugging it switches into perspective view. 

So, far I no further ideas what to share.

Pavel A.
Dec 15, 2025 9:38 PM UTC

Just keep in mind that Serial port is an exclusive device in Windows. Only one program (or widget or thread or instance , whatever it's called) can open the port at any time. Other attempts will fail with access denied. 

 

AScha.3
Super User
Dec 14, 2025 9:31 AM UTC

Hi,

if the serial (IDE) console looses connection : check if the system (Win11 here) causes this, just open new -> serial console -> new...and see, what the system offers to connect (the small down arrow )

AScha3_0-1765703809751.png

Then open with new name with this port.

I had this also sometimes, but dont ask me when it happens (on Win and Linux - same), long time ago ;

on IDE 1.18.1 here, same on 1.17. , 1.19. , just 2.0. not using , so dont know; but should be same.

btw

I always use the built in console ; its nice to see whats going on one or even on more than one connected boards,

while editing the program(s) , on the same screen.

AScha3_1-1765704616912.png

 

If you feel a post has answered your question, please click on " Best Answer ".
Associate II
Dec 15, 2025 9:32 PM UTC

@AScha.3 wrote:

Hi,

if the serial (IDE) console looses connection : check if the system (Win11 here) causes this, just open new -> serial console -> new...and see, what the system offers to connect (the small down arrow )

AScha3_0-1765703809751.png

Then open with new name with this port.

I do not get that far. When I try to open a new console I get the error message

Screenshot 2025-12-15 222933.png

Associate II
Dec 15, 2025 9:48 PM UTC

Just to add, I do not have this problem when I use Tera Term only.

EDIT: so TeraTerm seems not be getting confused by starting and terminating a debug session, while the IDE does. That's why I think this looks like a bug in the IDE.

 

DSebastianAuthorBest answer
Associate II
Dec 15, 2025 10:24 PM UTC

ooooooooooooooooooooohhhh. I guess I found my mistake (aarrg, why the icons in STM32CubeIDE are so small) - so I had a look on the linked discription again where it was said:

"This also works while in debug mode and you can switch the “Console view” by clicking and expanding this icon"

... I thought the icons are the same. But actually the are not.

So, for the very first connection (either in editing or debug mode), one has to click on this icon (sorry for screen shots again):

Click on "3 Command Shell Console"Click on "3 Command Shell Console"

Then, once the connection is established, one need to select the console to display for any further view by clicking on the icon just left to it and select it (screen shot below).
Under 3 the connected Nucleo_L432 (name I have choosen) an be selectedUnder 3 the connected Nucleo_L432 (name I have choosen) an be selected

I leave the pictures large to see the icons in a better way.

... and now I don't know where to place the solution marker. Thanks to Andrew Neil and Pavel A!

Andrew Neil
Super User
Dec 16, 2025 10:40 AM UTC

@DSebastian wrote:

I don't know where to place the solution marker. 


Well, your post describes the solution - so mark that.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.