STM32CubeIDE suddently stop to Debug and Run
Hi there,
I'm facing a problem with Cube IDE (ver. 1.13.0). Completely out of nowhere, it stopped letting me debug or run the code. When I click the buttons, I can see in the bottom right corner that it tries to launch the debugger, but it stops at Launching XXXX Debug: 0% and immediately disappear.
I already tried to reinstall everything, but nothing happened. I also tried to start the GDB server manually but nothing...
Actually, the board and ST-Link (V3MINI) are OK, and I can program the board through STM32Programmer.
Can anybody please help me? I can't work like that...
Thanks
Simone