STM32CubeIDE stops working after waking up on debian/ubuntu
I've had this problem for months now, in Debian 12/13(and Ubuntu 20.04), if I suspend my PC while STM32CubeIDE(1.12 to 1.14, both generic linux and debian versions) is running, when I wake up the PC and log in, STM32CubeIDE is completely freezed, I don't get any pop ups or warnings. The OS keeps workling perfectly, but the IDE doesn't respond, if I want to keep using it I have to kill the java process and reopen it, which has lead me to losing some work 2-3 times. I haven't found a report like this anywhere, am I doing something wrong? If not, is there a fix for this? Will I have to wait for next version to release?