Skip to main content
Alex Golubev
Associate III
January 24, 2022
Question

stm32cubeide + Srecord issues a warning calculation has at least one hole

I'm making a bootloader. Need a checksum calculation

Connected to stm32cubeide Srecord to receive CRC.

Sprecord works according to the following script:

# srec_cat command file: srec_crc_dump_to_file.txt
#===============================================
#-disable-sequence-warning
#Input file
PLK.hex -Intel
#Fill hole with 0xFF
-fill 0xFF 0x8000000 0x08040000
#CRC Algorithm at given address
-STM32 0x08040000
#-crop 0x08040000 0x08040004
-Output_Block_Size=16
#Produce output
-o PLK_SRECORD.hex -Intel

After executing the script, I get a warning from S record:

srec_cat: PLK.hex: 47492: warning: The data presented for STM32 calculation has

  at least one hole in it. This is bad. It means that the in-memory

  calculation performed by your embedded system will be different than the

  calculation performed here. You are strongly advised to use the "--fill 0xFF

  --over <inoput>" filter *before* the STM32 filter to ensure both

  calculations are using the same byte values. See srec_info(1) for how to see

  the holes.

 I ask for help

This topic has been closed for replies.