Skip to main content
FedeRico1
Associate II
October 7, 2019
Question

STM32CubeIde resets include paths when build hardware project

Hi there,

I'm using STM32Cube Ide to work wih my STM32F7.

I really like this software also for the integration of STM32CubeMX.

I use the STM32CubeIde to configure the hardware, peripheral, OS and so on but when I build the configuration I noticed that also the Include Path are restore.

So every time I change a perpheral setting and I rebuild the the project, the project lost the setting and I need to add manually every source folder that I added.

Is there a way to avoid this?

Thanks for the help.

BR,

Federico

This topic has been closed for replies.

4 replies

Cartu38 OpenDev
Graduate II
October 15, 2019

Definitively a bug.

Sounds some improvements have been done Thanks STM32CubeIDE V1.1.0 just released on st.com

JKlyn.1108
Visitor II
November 8, 2019

For me, 1.1.0 has problems on MacOS. I cannot get ST-Link debug to work, only OpenOCD. 1.0.2 works fine (except the bug above, very annoying!) These tools are rather disappointing.

Cartu38 OpenDev
Graduate II
November 8, 2019

"1.1.0 has problems on MacOS" what do you mean ? Is such still related to "resets include paths when build hardware project" i.e. your post header or MacOS issues in general relying on 1.1.0. If general 1.1.0 MacOS issue I obviously agree according numerous post about.

JKlyn.1108
Visitor II
November 11, 2019

I have the same problem as OP, and in addition, on MacOS, the ST Link debugging doesn't work. It does work on 1.0.2