Skip to main content
xpress_embedo
Associate III
October 27, 2022
Solved

STM32CubeIDE Register View Problem

Hello Everyone

I am using the latest STM32CubeIDE i.e. 1.10.1, and I am facing a strange problem.

In the register view of the Special Function Register, I have a problem.

0693W00000VOHdqQAH.pngAs can be seen above the RCC->CR register value is 0x30006783

This means that Bit 28 and Bit 29 are set, these bits are PLLSAIRDY and PLLSAION, but here it looks like some wrong mapping is done, these two bits are not shown in the SRF view

0693W00000VOHfDQAX.pngCan someone please suggest why this is happening, am I doing something wrong?

This topic has been closed for replies.
KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
October 28, 2022

Hello @xpress_embedo​,

Thank you for bringing this issue our attention.

I confirm the issue: The 28 and 29 bits filed for the RCC_CR register are missing in the STM32F429.svd file.

I reported internally.

Internal ticket number: 137645 (This is an internal tracking number and is not accessible or usable by customers).

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

8 replies

waclawek.jan
Super User
October 27, 2022

Which STM32?

JW

Tesla DeLorean
Guru
October 27, 2022

Provide more details.

The .SVD files seem to have a lot of issues with completeness / correctness. These are used to describe registers, and bit level content.

@KDJEM.1​ 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
xpress_embedo
Associate III
October 27, 2022

Hi @Community member​ 

The STM32 is STM32F429Z and I am using STM32F429I-DISC Board, this information was shared in the image attached in the main post.

0693W00000VOHfDQAX.pngHi @Community member​ Can you please tell me what information is needed from my side?

Pavel A.
October 27, 2022

Per-bit decodes of bits 28-29 are missing. It ends at 27. Nothing is wrong, just incomplete.

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
October 28, 2022

Hello @xpress_embedo​,

Thank you for bringing this issue our attention.

I confirm the issue: The 28 and 29 bits filed for the RCC_CR register are missing in the STM32F429.svd file.

I reported internally.

Internal ticket number: 137645 (This is an internal tracking number and is not accessible or usable by customers).

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
xpress_embedo
Associate III
November 6, 2022

Thank You

KDJEM.1
ST Technical Moderator
August 25, 2025

Hello @xpress_embedo ,

 

The issue is fixed in https://www.st.com/resource/en/svd/stm32f4-svd.zip version 2.0.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.